Part Number: J721S2XSOMXEVM Tool/software: As per TISCI documentation , it supports keyring functionality which help import additional keys which can be further used to authenticate images. Generating keyring blob involves a lot of complex steps, do we…
Part Number: J722SXH01EVM Other Parts Discussed in Thread: SYSCONFIG Tool/software: The J722SXH01EVM has a 40 pin header and a few McSPI interfaces are routed to this header? How to enable the pins for McSPI?
Part Number: PROCESSOR-SDK-AM64X Tool/software: Greetings,
For a use case, where characters are received via UART RX, we define the UART Transaction parameters.
In the UART Transaction parameters, we define .count as well, which denotes the number…
This is a companion FAQ for
[FAQ] [Alert] DM R5F can crash in certain conditions: AM62x, AM62Ax, AM62Dx, AM62Px, AM67, AM67A
Please read the alert first. You can also find more information in the main FAQ here:
[FAQ] DM R5F can crash in certain…
Other Parts Discussed in Thread: AM67 , AM67A
This is a companion FAQ for
[FAQ] [Alert] DM R5F can crash in certain conditions: AM62x, AM62Ax, AM62Dx, AM62Px, AM67, AM67A
Please read the alert first. You can also find more information in the main…
Part Number: BQ25600 Other Parts Discussed in Thread: BQ25601 Tool/software: The /QON pin has multiple functions on the BQ25601/D and BQ25600/D and is pulled up internally. The only thing connected to this pin should be some switch/FET/button etc. Float…
Part Number: BQ25600 Other Parts Discussed in Thread: BQ25606 , , BQ25601 Tool/software: When a fault occurs on BQ2560x (excluding BQ25606) an /INT pulse is sent to the host. For the BQ25601/D and BQ25600/C/D the fault statuses in REG0x09 are kept static…
Part Number: BQ25600 Other Parts Discussed in Thread: BQ25601 , Tool/software: The I2C programmable BQ2560x has a mode to minimize quiescent current for the BQ25601/D and BQ25600/C/D from the battery in cases when the system load is not needed to be powered…