FAQ: TPLD > Current FAQ
The two biggest causes of slow simulation are:
Fast oscillators and switching signals
Large simulation timescales (simulations that take 1+ seconds)
If the simulation is utilizing a square wave with a period that is…
FAQ: TPLD > Current FAQ
Numerous TPLD products are either pin to pin or layout compatible with competing products. Our products utilize standard, JEDEC packaging standards.
FAQ: TPLD > Current FAQ
Once a TPLD is permanently programmed or “burned” through OTP, the design cannot be changed. If you wish to change your design after permanently programming an OTP part, a new, previously unprogrammed part must be used.
FAQ: TPLD > Current FAQ
TPLD is programmed through SPI communication enabled by the programmer firmware and InterConnect Studio (ICS). Each TPLD device uses 5 pins to program the device: 4 pins for SPI communication and 1 pin (GPI) that provides a specific…
Other Parts Discussed in Thread: TPLD1201 FAQ: TPLD > Current FAQ
TPLD is programmed through our software tool, InterConnect Studio (ICS) , in combination with a TPLD programmer and EVM. TPLD programmers and EVMs can be found on the “Hardware development…
FAQ: TPLD > Current FAQ
No, current devices do not support in-system or inline programming (support is planned for future devices). For large scale production, we recommend you have TI program the devices before shipping. Customers can program devices…
FAQ: TPLD > Current FAQ
Customers can order devices for production through InterConnect Studio (ICS). TI can program devices (at no additional cost!) before shipping with the submitted design if the order quantity is one reel or more (3000 units). …
FAQ: TPLD > Current FAQ
TPLD uses Floating-Gate One-Time Programmable (OTP) technology to program its parts, as opposed to other Non-Volatile Memory techniques such as eFuses or AntiFuses, or Volatile Memory technologies such as EEPROM or RAM.
Floating…
FAQ: TPLD > Current FAQ
TPLD stands for TI Programmable Logic Devices . These devices are a family of programmable logic devices integrating multiple digital and analog functions into a single small package.