Part Number: AM62D-Q1
By default, The AWE SDK uses the AWE Designer to load any signal processing chain. However, once the signal chain is finalised, how to load the signal chain on startup without the use of AWE Designer?
Part Number: TMP103
Hello Team,
Regarding the TMP sensor family, are they able to run at 100kHz as named ‘Standard Mode’ in the I2C standard? If so, are all the sensor specifications compatible with the I2C standard?
Part Number: TMS320F2800137 Other Parts Discussed in Thread: C2000WARE
Hello,
I want to port the E-Metrology library fom F28P55 to F2800137. I want to enable only single-phase calculations and I do not wish to calculate THD. What steps can I follow…
Other Parts Discussed in Thread: AM2431 Hello Randy
AM2431: MCU design: PCIe differential impedance value
Since the 2 queries are 2 different topics, i will split the thread.
For PCIe interface traces impedance control, I get different information…
Part Number: BQ25188 Other Parts Discussed in Thread: BQ25185
TS pin operation
The BQ2518x uses an internal 38uA current source on the TS pin to bias the NTC thermistor, and the resulting TS voltage is compared against internal reference voltage thresholds…
Part Number: AM620-Q1
There are more than 30 ECC aggregators in each of AM62x, AM62Ax, AM62Px and AM62Dx devices. How do we find the ESM events corresponding to each of the ECC Aggregators?
Other Parts Discussed in Thread: AM625 To successfully bring up a custom AM625 board, the primary objective is to establish a minimal Device Tree (DTS) to serve as the baseline for the board port. This FAQ is designed to guide developers through the creation…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: AUDIO-AM275-EVM , AUDIO-AM62D-EVM , SK-AM62A-LP
Can you let me know the steps I can use to reduce the CAN response time using MCU+SDK/FreeRTOS SDK and the method to measure this time?
Part Number: AM625 Other Parts Discussed in Thread: UNIFLASH
Greetings,
Here is a list of all the OSPI/SPI/QSPI FAQs for Sitara MPU Family of devices.
Please choose the FAQ which is the most relevant to your issue/failure/doubts.
Note: xSPI Custom…