Part Number: TPS65072EVM-430
I would like to purchase TPS65072EVM to get exposure on PMIC .When i am trying to get the user manual of TPS6507X EVM software i could not able to get.And i would like to know what kind of tests i can perform on this EVM…
Part Number: LP8758-E0 Other Parts Discussed in Thread: LP8758
I got the answer that LP8758-E0 Max duty is 100% from the following URL E2E post.
However there is "dropout voltage" (min 0.7V) on datasheet electrical characteristics.
What does this…
Part Number: TPS65070
I'm using the TPS65070 as Power-Manager of an IIoT-System. As power-supply I use LiPo or/and AC. After booting the TSP EN_DCDC1 is high and in the CON_CTRL1-Register there is the default setting “01111111” This means after pulling…
Part Number: ADS1282
Hi all,
For unipolar mode (AVDD=5V, AVSS=0V, VREFP=5V, VREFN=0V), ADS1282 full-scale input voltage is from 0V to 2.5V. Am i right?
Also data code is range from 00000000h to 7FFFFFFFh for FIR filter. Am i right?
Most of…
Part Number: TIDM-THREEPHASEMETER-F6779 Other Parts Discussed in Thread: MSP430F6779
With Reference to the reference design:
SLAA577G–January 2013–Revised August 2015 Implementation of a Three-Phase Electronic Watt-Hour Meter Using the MSP430F677x…
Part Number: MSP430F5528
Hi,
Can someone clarify what temperature range the TLV ADC gain and offset parameters were intended for? Were these TLV parameters optimized from -40C to 85C or
at room temperature only?
-Kelvin
Dear MSP community,
The complexity of applications is increasing, and the integration of functions on a single chip is also increasing. Therefore it is natural that dedicated functions sometimes do not work as a developer expects.
In such cases…
Part Number: BOOSTXL-DRV8323RS BOOSTXL-DRV8323RH Other Parts Discussed in Thread: DRV832X , MOTORWARE , LAUNCHXL-F28027F , , LAUNCHXL-F28069M , BOOSTXL-DRV8323RH
We are not planning to revise MotorWare from the current v18. However, many of our customers…
Part Number: DLPLIGHTCRAFTER
Getting the DLP® LightCrafter™ EVM to work with Windows 10
In order for the DLP LightCrafter EVM to work with Windows 10 the default driver needs to be replaced. Below is one driver that can be used for successful operation…
Part Number: DLPDLCR2000EVM
All,
We would like to present a brief tutorial on how to get your DLP® LightCrafter™ Display 2000 EVM up and running on a BeagleBone Black. This tutorial will assume limited Linux/Debian experience. For more general information…