Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP-FET I have a new MSP430 board that is not booting. This was a working design with the previous board. As far as I can tell it has power and I am able to program it with the MSP-FET. That…
Part Number: MSP430FR59941 Other Parts Discussed in Thread: MSP-FET , MSP430FR5962 , MSP430FR5964 , MSP430FR5994 , MSP430FR5992 , When I have the MSP-FET connected to the MSP430, the chip responds properly to low reset pulse. The chip resets and starts…
Part Number: LM3549 Reg 40h EEPROM CONTROL
When Reg 0x40 is set to 0x04 does the PROM get set with the default register values or does it clear the EEPROM (all zero/ones)?
Regards,
William
Part Number: LM3549 When I enable the chip (EN=H) how long must I wait for the chip to come alive? (How long does it take to get to Standby?)
How do I know when the part is ready for use? (EEPROM-> reg is complete,... I can now enable an LED)
Regards…
Part Number: LM3549 Reg 0x14
Enables soft start feature and selects soft start time.
What is the purpose of the Soft Start feature? Why would I want a short Soft Start time? Why would I want to have any Soft Start time?
How does this effect the…
Part Number: LM3549 Reg 0x15
ILIMIT register sets the buck-boost converters current limit values.
The datasheet makes no mention of the use of these values? i.e. Why would I limit the current to 2Amps when the part can only deliver 700mA max?
Please…