Hi.
Usb2Uart adapter was buggy. It was be replaced with new.
Connection between TDA2P:Porz(in)/RstOut(out) and 917_A54:WarmReset(in)/RstOut(out=Porz) was be corrected.
Now AsicID is always 70 bytes.
See attached picture (dump from start).
Yes…
Hi, Brijesh. How about Line-Concatenated Mode?
For example. The 1st UB962 combine 4 frames from cameras to one big metaframe. The 2nd UB962 combine 4 frames from cameras to another big metaframe. In this case I need to de-Bayering only two frames. Finally…
Hi. Thank you for answers. We made a mistake in 962 Two-DL config. We fixed config both for CSI2 trasmitter and receiver. Today we tested UB962 with custom TDA3-board using 2DL config. It works with 4 cameras, but sometimes freezes occur when watching…
Part Number: TDA2P-ACD I am designing pcb of TDA2PHFUQACDQ1 with O9039A385IZWS.
I have a question about 1.8V LDO powered balls.
vdda_abe_per(N9,P16), vdda_mpu(P18), vdda_gmac_core(R15), vdda_video(R14), vdda_ddr(N19), vdda_debug(N13), vdda_dsp_eve…
Hi, Natasha.
The problem is usage of latest 919/otp52 with TDA3 in context of power-management.
I'm sorry for little big text. Let's me explain the situation. Side (A) is PMIC919/otp52. Side (B) is TDA3.
1) Host (PC) starts and wait for TDA3(uart…
Part Number: TDA2P-ACD Other Parts Discussed in Thread: TDA2 , DRA77P Hi.
(1) There is no mech.drawing of ACD(784-balls)-package in datasheet.
Do I need to use ABC(760-balls)-package drawing as reference for my design? (Does it have the same size…
Hi,
TDA3 has dual C66x core.
TI has H.264-encoder implementation for C66x cores.
Can you explain why H.264 is not possible, but only mpeg4? Is this a speed or memory limitation?