Part Number: 66AK2G12 Hello,
I am a beginner of TI processor and device tree. I am puzzled by the "interrupts" property of device tree of 66AK2G Processor.
For example, in /arch/arm/boot/dts/keystone-k2g.dtsi ( https://elixir.bootlin.com/linux…
Part Number: 66AK2G12 Other Parts Discussed in Thread: LM63 Hi,
We are using LM63 as our temperature sensor and fan control chip. There are many sysfs files that the lm63.c driver can export. However, on our system which uses TI 66AK2G12 CPU, only one…
Hi Tom,
let me take a stab at this. Just as a disclaimer, I never worked on this legacy platform, and also don't have access to it, so my comments here are based on looking at the documentation and kernel sources (untested).
Tom Chen said: &spi1 {…
Part Number: 66AK2G12 In the datasheet, VIH DDR3_VREFSSTL +0.09V and VIL DDR3_VREFSSTL -0.09V are described as 0.765V/0.585V respectively, but why are they described as follows?
In case of [Model] PDDRIO_D3FP3L_34 Vinh = 810.000mV Vinl = 540.000mV
[Model…
Part Number: 66AK2G12 Hi,
When it works under ambient temp 70C, top case temperature is 110C.
It works well but junction temp range is from -40C to 105C.
Can it be used under this condition?
Thanks.
Hi,Experts
Currently the GPMC multiple read/write is not working, any advice? GPMC single read/write is working. We are trying to get GPMC multiple read to work first.
- NOR Flash like, asynchronous and synchronous devices - Non-multiplexed attached dev…
Part Number: 66AK2G12 Other Parts Discussed in Thread: EVMK2GX , My EVMK2GX board uses MT41K512M8DA-107 (DDR3L) parts, which is speed grade 1866.
The spreadsheet will only let you choose 800, 1066, 1333 or 1600, and it is password protected, and won't allow…