Part Number: 66AK2H06 Other Parts Discussed in Thread: TCI6638K2K Tool/software: Hello all, We are working with TCI6638K2K keystone II processor and encountering intermittent SRIO communication issue with our FPGA. We would like to simulate our SRIO interface…
Part Number: 66AK2H06 Tool/software: Hi experts,
I have a question about the IPC function of the 66AK2H06DAAW2.
Q1. Is it okay to use an IPC interrupt that targets the core itself? (In the datasheet "10.2.3.13 IPC Generation (IPCGRx) Registers", it…
Part Number: 66AK2H06 Tool/software: Hi,
1) Recently, an exception occurred in on-site devices. The relevant exception information is as follows. We have simulated various exception tests but failed to reproduce the same exception record information…
Part Number: 66AK2H06 Tool/software: Hi
Recently, a device using a 66AK2H06 processor reported a single-bit error in the SL2/MSMC memory that persisted. We have conducted simulation tests and would appreciate your feedback and follow-up as soon as possible…
Part Number: 66AK2H06 Tool/software: Hi,
We have two Ethernet port in our HW with 66K2H06.
one of the Ethernet address is assigned from the U-boot. I am wondering how do I add the second ip address and let Linux kernel recognize it?
Do you have…
Part Number: 66AK2H06 Tool/software: Dear Sir,
I install ti-processor-sdk-linux-k2hk-evm-06.03.00.106 and run setup.sh under install directory.
it generates the file: arago-base-tisdk-image-k2hk-evm.ubi
However, I check k2hk_evm.sh, it need file…
Part Number: 66AK2H06 Tool/software: Hi,
I have question about CCS.
There is Pre-build steps under Build. is it possible I can execute a python script there before building my code?
Thank you
Yao-Ting
Part Number: 66AK2H06 Tool/software: Hi,
When I build the Linux kernel for 66AK2H06.
How do I assign 2 cores information to the boot-image?
Thank you for your time.
Yao-Ting
Part Number: 66AK2H06 Other Parts Discussed in Thread: 66AK2H12 , TCI6638K2K , TCI6636K2H Tool/software: Could you tell us whether the device itself controls the switching of High→Low for DDR B Reset pin?
If yes, what kind of triggers are there?
…
Part Number: 66AK2H06 Hi experts,
My customer is running Linux on a 66AK2H06 ARM. Recently, upgraded the Linux Kernel Version from 3.10.72 to 4.19.94, but a problem is occurring with PCI. Regarding Linux updates, instead of updating only the kernel…