Hi,
I am working on Keystone 2 platform based board. U boot is up on the board and network(eth0) is also working. I am trying to get linux, filesystem over network using DHCP. When I run dhcp it always gives below output.
uboot#dhcp BOOTP broadcast…
Hi Karthik,
thank you for your kind reply. I've already changed the dtb, but I to be sure I redid it again.
So far nothing good, I get the same error as before when I insert debugss.ko module:
[ 124.961850] ERROR: could not get clock /soc/debugss…
I have been trying to setup A66AK2H EVMK2H board to boot up using the TFTP/NFS setup as suggested by the user guide, but I'm having trouble getting NFS to work.
The kernel image is loaded correctly using TFTP and appears to boot successfully. However…
Hi,
I am trying to do some tracing/profiling using Keystone 2 based EVM with CCS 5.5 and XDS200 onboard emulator but I am getting the following error from CCS:
"Could not run analyzer on C66xx_0. Cause: Channel driver is not availabe. CPU is not selected…
Version of MCSDK - MCSDK_HPC_03_00_01_08 Processor and board platform (EVM & its revision) - Hawking chip Evaluation Board EVMK2H Rev 3.0.
API - OpenCL 1.1, no CSL
Hello everyone,
Very specific question: the openCL code was compiled with the options…
Hello
I encountered a problem when i run openCL code on EVMK2H .
I have attempted to run TI openCL examples which can show some platform information ,and the results show the Device operate at 0.059GHz frequency
As I know,AK2H12/14 SOC have…
Other Parts Discussed in Thread: OMAPL138 I'm attempting to run a benchmark of the ARM Cortex-A15 core on the C66AK2H12 in comparison with the OMAPL138 Cortex-A9 core, both on bare metal. The L138 was easy enough after downloading the Starterware package…
Other Parts Discussed in Thread: 66AK2H06 , 66AK2H12 Hi expert,
3.0 devices can read/write normally mounted as a non-root device with always reset information. And more worse, it does not always boot successfully when we use USB 3.0 flash disk as root…
Hi Sahin,
I tried it again, but it's always the same result. Something is missing.
The output from the command line:
Fullscreen
7433.pdfProjectCreate_withSetup.txt
Download
C:\WINDOWS\system32>cd C:\ti\pdk_omapl138_1_0_4\packages…
Part Number: EVMK2H Other Parts Discussed in Thread: 66AK2H12 , SYSBIOS Hi,
I have recently bought EVMK2H board and i have tried bare metal examples on ARM using GNU v4.9.3 compiler as well as DSP using TI compiler.
Now i am trying to build the…