Part Number: 66AK2H14 Tool/software: Hi Community members,
Inside the SPRUHJ5 document we can find the "RXDMAOVERRUNS" register from the statistic module.
They are located at offset 0x188C for Lane 0 and 0x1A8C for lane 1
The document only "explains…
Part Number: 66AK2H14 Tool/software: Hi Community,
I would like to understand the Serdes Tx parameters based on the spruho3b document.
§14.2.3 declares 4 parameters C0,C1,C2,CM where C0 is calculated from the CM,C1,C2 values. Equation (3) gives…
Part Number: 66AK2H14 Tool/software: Hi All,
We have been using the 66AK2H14-based board for quite some time and are planning to upgrade the kernel version.
The latest supported TI-Processor SDK release version is "k2hk-evm-linux-sdk-src-06.03.00…
Part Number: 66AK2H14 Tool/software: Restarting programming DSPs after few years, it is not clear which is today the recommended design environment, like ccs version, win/linux, etc.
Any suggestion?
Part Number: 66AK2H14 Tool/software: Hi,
For the Keystone2 (K2HK) board, the subsystems like the SRIO, netcp, hwqueue & pktdma need drivers, among which only the SRIO driver is not there in the upstream 6.6 kernel, rest all the other drivers are present…
Part Number: 66AK2H14 Tool/software: Hi,
We're trying to combine a NIMU application for our custom 66AK2H14 design based on EVMK2H EVM NIMU example .
In case of EVMK2H all SGMII[0,1,2,3] ports are routed (#0 / #1 through PHY to front panel and #2…
Part Number: 66AK2H14 Tool/software: Hi All,
We are into development of custom 66AK2H14 board based on 6.x Linux kernel, We are looking out for the latest keystone rapidio driver.
We could not find the keystone rapidio driver from the latest TI-supported…
Part Number: 66AK2H14
Tool/software:
Hi,
My question is about de 10G PHYB serdes
The 66ak2h14 provides 2 lanes capable of running at 10G and 1G
Is it possible to run one lane at 1Gb/s and the other at 10 Gb/s ?
with best regards, …
Part Number: 66AK2H14
Hi all,
Did someone succeeded to make MT29F1G08ABBFAH4-ITE:F NAND flash work with any C66x design?
Our design is based on 66AK2H14 SoC and MT29F1G08ABBFAH4-ITE:F NAND flash.
Previously we were using MT29F1G08ABBDAH4-IT…