Part Number: ADC1175 Support Path: /Product/Device selection assistance/ Hello,
I have an application for an 8-bit ADC, but it is low-speed. I like the specifications of the ADC1175 because of it's parallel output and two reference voltage inputs. …
Hi Cherry,
This question was already posted by the customer and answered at https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1195461/tm4c1294kcpdt-when-i-use-the…
Other Parts Discussed in Thread: ADC1175 For some reason my parralel ADC ( adc1175 ) cant read continuously, every time i want to read a new value, i have to turn it off and on.
I left the output enable connected to ground. Im using this schematics except…
Other Parts Discussed in Thread: ADC1175 , LMV796 , LMH6702 Hi,
The ADC1175 has a dynamic capacitive load (4pF when the clock is low and 11pF when the clock is high). Is this why there is a 62pF capacitor in the reference circuit on page 16 on the datasheet…
Part Number: ADC08060 Other Parts Discussed in Thread: ADS831 , ADC1175 , Hello
It is mentioned in adc08060 (adc1175, ads831, etc) datasheet that the output data is valid just after the rising edge of the clock, does it mean to read the data with rising…