Part Number: ADC12020 Dear Expert
At present, the impact of temperature on the measurement accuracy of this ADC is only analyzed in a positive direction
It is best for the manufacturer to provide an analysis report on the measurement accuracy of ADC…
Part Number: ADC12020 Other Parts Discussed in Thread: LMH6550
Tool/software:
In the ADC12020 DataSheet, figure 40 shows an example circuit of the chip, in which a differential driver circuit is used. The driver circuit uses LMH6550 with a Vcm end…
Part Number: ADC12020 Tool/software: Dear Expert We use singel end input ,and use REF5020 as 2.048V ref voltage,now we test found that the offset error is too high.
And different IC could have different offset error.
Below is schmetic ,could u…
Part Number: ADC12020 Hi,
I find from the datasheet that "Conversion Rate 20 MSPS (min) " and "the lowest sample rate to 100ksps" and "100 kHz ≤ fCLK ≤ 30 MHz "
I want to know the minimum sample rate of ADC12020, is it 100ksps?
Thank you for your…
Part Number: ADC12020 Sheet 8, Maximum clock frequency:
25C typical 20MHz
Over temperature 30MHz
Are these reversed? All other 25C specs are better than over-temp specs (as we would expect).
Part Number: ADC12020 Hi Team,
My customer s looking for the complete thermal data for the device ADC12020, I've checked the datasheet and it seems the information listed is limited. Can you share the complete thermal resistance data of this device…
Part Number: ADC12020 Hi, team.
I would like to know the method to set the trigger for data conversion in ADC12020. Could you please let me know how to start sample & hold with arbitrary timing?
Regards, Nagata.
Part Number: ADC12020 Hello,
We are evaluating ADC12020 for a new product development. The characteristics of the input to the ADC is as follows:
1- Single Ended 2- 0 to 4.15 volts p-p
In order to avoid saturation of the ADC12020 can TI confirm…
Other Parts Discussed in Thread: ADC12020 , TVP7002 Can someone provide guidance on how video image processing ICs like the ADC12020 and ADV7179 would be interfaced to the C6A integra series (i.e. p/n TMS320C6A8168)? I've seen HPI (High Performance Interface…