Part Number: ADC121S101 Dear Champions,
I'm looking for ADC with spi interface, and belows are my requirest. I have considered with using ADC121S101, but this is i2c interface, and my MCU can't support run above 1Mhz for i2c's CLK. So I plan to see…
Part Number: ADC121S101-Q1 Hi TI-team
My customer have some question.
There is a notation "VA + 0.3V" on the data sheet.
And D1 is connected to the equivalent circuit of Fig.19 on P.14 as a protection.
When an overvoltage is actually applied…
Part Number: ADC121S101 Hi Team,
My customer is using ADC121S101 in their design. The problem is that ADC121S101's digital output is double of input voltage.
For example, if the input voltage is 1V, the digital output should be 1/3.3*4095=1241. But…
Part Number: TMUX1308-Q1 Other Parts Discussed in Thread: TMUX1308 , AM625 , TMUX1308A , SN74LV4051A , TMUX1308A-Q1 , ADC121S101 , , TPS65224-Q1
Tool/software:
Hi Team,
TMUX1308 EN and control A0..A2 is being controlled by AM625 Sitara SOC.
SOC IO buffers are…
Part Number: ADC121S101-Q1 Other Parts Discussed in Thread: ADC101S101 , ADC121S101 Please inform Offset and Gain Error for 5V supply.
I could only find the values for 2.7V to 3.6V range in the datasheet (item 7.6).
Best Regards.
Edson
Part Number: ADC121S101-Q1 Hello
My question is, for the ADC121S101-Q1, what is the value for INL and DNL, considering power supply ranges up to 5V? The datasheet shows only these values up to 3.6V, but I am working with 5V and need INL and DNL for…
Part Number: ADC121S101 hi My customer would like to know why the current calculated is higher than measured at the input of the ADC (Vin) with 1Mhz SWITCHING CAP.
regards,
kamal
Part Number: SN74CBTD3384 Other Parts Discussed in Thread: ADC121S101 , Hi expert,
Customer connects 1 CH (pin10) of SN74CBTD3384 with 3 nCS pins of 3pcs of ADC(ADC121S101) together. Sometimes this channel fails (pin10 shorten to pin20, that is shorten to…
Other Parts Discussed in Thread: ADC121S101-Q1 , ADC121S021 Hello,
ADC121S101-Q1 INL, DNL, Voff and GE is specified at Fsclk is 10MHz to 20MHz as follows.
But Clock frequency of Recommended Operating Conditions is 25kHz to 2MHz.
Customer want to use…