Hi Taemin,
Yes, it is possible to change the sampling rate (1.5 to 3 GHz). Are you using the ADC32RF80EVM? There are some preset frequencies that can be generated by the onboard LMX2582. Additionally, you can use an external clock source (along with…
Part Number: ADC32RF80
hi team:
We have a block ADC32RF80EVM development board for use with the TSW14J56EVM. There are a few questions:
1. ADC32RF80 is 14 bits, the peak-to-peak value is 1.3V, and the full-scale count is 16384. But to use DDC, I set…
Other Parts Discussed in Thread: LMX2582 , ADC32RF80EVM , LMK04828 i
I have a question about configuring LMX2582. The chip is palced on the evaluation board ADC32RF80EVM and I try to get 3GHz from LMX2582 outputs. His input frequency = 122.88MHz (get from…
Part Number: ADC32RF45 Other Parts Discussed in Thread: ADC32RF80EVM , ADC32RF80 DEARS.
Power detector related questions.
The customer designs and tests its own board.
The version of ADC32RF80EVM is Rev E.
The Power Detector Register(5400h) Setting is on…
Part Number: ADC32RF45 Other Parts Discussed in Thread: ADC32RF80 , ADC32RF80EVM Dears.
We are testing the ADC32RF80.
The test settings completed are as follows.
Sampling : 2949.12Mhz
Decimation : 6
BW : 300Mhz
LMFS : 4421
Sysref : 3.906Mhz
K=32.
I changed…
GSG_Lamarr_ADC32RFxx.docx Eran,
In discussing with HSP team, the ADC32RF80 EVM has high power input requirement for clock source. Although -4dBm clock worked in our system, it's at a marginal level. To minimize the loss, the SMA cable used for clock should…