Part Number: ADC3444 Other Parts Discussed in Thread: ADC3442 , Dear Forum members.
Could you please comment on the following?
Is there a graph available detailing the power consumption on the analog and digital rails versus the sample rate?
For…
Oops, The quad ADC is an ADC3442, not LT1550. Please disregard the LT1550. I would like to know though if this or another quad ADC can interface to the TMS320C6655. Thanks.
Part Number: ADC3441 Hello,
in the datasheet for ADC344x pg. 46, 9.3.1 Analog Inputs section it says that
Each input pin (INP, INM) must swing symmetrically between (VCM + 0.5 V) and (VCM – 0.5 V), resulting in a 2-VPP (default) differential input…
slau579d.pdf Leejh,
Connect a 80Msps clock (or lower) to SMA J9 with a power of at least 10dBm. See section 1.4 and figure 7 of the attached ADC3423EVM User's Guide.
Regards,
Jim