Part Number: ADS124S06 Other Parts Discussed in Thread: ADS124S08EVM , ADS124S08 I am having difficulty obtaining linear ADC readings from the ADS124S06. I am able to setup the ADS124S06 correctly as I did with the ADS124S08EVM board. The settings are…
Part Number: ADS124S06 Hi there,
We have selected ADS124S06 for Bridge sensor.
Bridge sensor specifications:
1. Excitation voltage : 3.3V
2. Sensitivity : 2mV/V
3. Capacity : 2Kg
Our required Programmable data rate is 2000kSPS .
By setting this, We are…
Part Number: ADS124S06 Hello,
My customer has a question for ADS124S06.
When there is no external available clock but CLK bit in Data Rate Register is wrongly set to use external clock, can the device be reset by /RESET signal?
The datasheet specifies…
Part Number: ADS124S06 Other Parts Discussed in Thread: ADS1120 , ADS1220 , ADS114S06 Hi Sirs,
Please help on these questions.
Thanks.
1. While using single-end input, the int. PGA needs to disable or not? And if disabled the PGA, what the input impedance…
Part Number: ADS124S06 Hello,
ADS124S06 datasheet recommends to tie unused GPIO output pins to AVSS through a pulldown resister and set the output to 0.
ADS124S06’s default setting for GPIO pins is output. So I don’t think there is any risk to leave…
Hi Obata-san,
Leakage current is a complex discussion. When connecting the analog input to AVSS the highest leakage current occurs at high temperature with the bulk of the leakage current coming from the ESD structures.
As an example, note the datasheet…
Part Number: ADS124S06 Hi,
ADC used is ADS124S06IPBSR and RTD used is PTS1206M1B1K00P100.
Could you please help back calculate the temperature from the known RTD resistance, as i am finding it difficult to calculate the temperature from the quadratic equation…
Part Number: ADS124S06 Other Parts Discussed in Thread: ADS1220 Hello,
My customer has a question for ADS124S06.
ADS1220 datasheet specifies wakeup time as 50usec. This time is required to wake-up from standby mode.
Is the similar wake-up time required…
Part Number: ADS124S06 Hello,
I have 2 questions for ADS124S06
1. About programmable conversion delay
My customer just wonder how much delay is appropriate for their system. I understand it highly depends on the system. But could you help how to think…
Part Number: ADS124S06 Hello,
The ADS124S0x datasheet specifies power consumption data with AVDD=DVDD=IOVDD=3.3V on P13.
But it is a little bit different from my customer’s case.
Their case is AVDD=5.0V, DVDD=3.0V and IOVDD=5.0V.
Do you have any…