Hi Kimon,
I reached out internally to the team, and they would like more information as to your issue. If you would like more assistance on this, please send the problem file and some captures of your debug.
In any case, I will be closing this thread…
Part Number: LCFILTER-CALC-TOOL Hello team,
I always had a confusion with the Inductor and ferrite bead in the power input line ( buck converter) and output line.
Please can you tell me when we have to use the ferrite bead over the inductor , what are…
Part Number: LM76005 Hi,
Value of output capacitor to use differs between datasheet calculations and WeBench tool. (ambient of 80C max.) Vin = 11 to 52 V
Vout = 5.667 to 5.881 V (using Rfb of 100k + 21k 0.1%). [Require Vout(min.) = 5.5 V and Vout(max.…
Hi Daisuke-san,
Daisuke Maeda said: Was a heatsink used for the AM62x on the board used for measurements in the application note?
There was not one used. Instead a Thermal Flow System, TFS.
Daisuke Maeda said: What is the airflow (m/s) under temperature…
Part Number: TMS320F280038C-Q1 Hi,
there is a power estimation tool available for F28004x -> https://www.ti.com/tool/C2000-F28004X-POWER-EST-CALC
Is there something available or planned for F28003x ?
Thanks and best regards,
Gregor
Part Number: ZIGBEE-POWER-CALC TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI…
Other Parts Discussed in Thread: ANALOG-ENGINEER-CALC I messaged TI and they said I should post here. Maybe with enough interest TI will update the ANALOG-ENGINEER-CALC tool. My suggestion is to allow entry of one of the calculated values. In the Passive…
Part Number: AFE7952 Hi,
I find out a good tool in TI; https://www.ti.com/tool/FREQ-DDC-FILTER-CALC
I set Fs=2900MHz, Interleave=1, Fc=2050MHz, BW=1MHz.
I get: Rx band=850MHz, HD2=1200MHz, HD3=350MHz, HD4=500MHz, HD5=1350MHz
"slyt738.pdf" The TI doc. show…
Part Number: AFE7952 Hi,
I find out a good tool in TI; https://www.ti.com/tool/FREQ-DDC-FILTER-CALC
I set on sheet-2 ; Fs=2900MHz, Interleave=2, Fc=2050MHz, BW=1MHz.
I get: Rx band=850MHz, HD2 image=250MHz, HD3 image=1100MHz, IL=600MHz
1: Interleace=2…