Other Parts Discussed in Thread: ADS1606 , OMAP-L138 , ADS1605 Original Thread : http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/12173/300324.aspx#300324
Hello Champs,
Can the ADS1606 EVM fit into the OMAP-L138 EVM…
Other Parts Discussed in Thread: ADS1606 If four ADS1606 ADC are tied to a common clock and taken out of reset at the same time, will all four ADC be in sync (phase)?
If four ADS1606 are running on a common clock, what is the best way to buffer / drive…
Part Number: ADS1602 Other Parts Discussed in Thread: ADS1601 , ADS1606 , ADS1605 , ADS1625 , ADS1626
What are recommended reference options for the ADS1601, ADS1602, ADS1605, ADS1606, ADS1625, and ADS1626 devices?
Part Number: ADS1605 Other Parts Discussed in Thread: ADS1606 , Dear Community,
I am looking for an ADC for a new application with 16 bits and a low INL (< +/- 1) and at least 2.5MSPS better 5MSPS
I found the ADS1605 and ADS1606 which are matching…
Other Parts Discussed in Thread: TMS320C6748 , ADS1606 , ADS1605 , OMAP-L138 Hi,
A customer is looking for hardware (EVM or alike) with an ADS1605 or ADS1606 on it, to be connected to a TMS320C6748 EVM for high speed data acquisition.
I checked the…
Other Parts Discussed in Thread: ADS1606 Hello,
I have for my study work the C6748 LCDK and ADS1606 EVM - 16bit analog-to-digital evaluation board
( http://www.ti.com/lit/ug/slau122a/slau122a.pdf ).
I´m seeking the best and easiest way to connect…
The internal voltage reference on the ADS1605 / ADS1606, V REF (V REFP - V REFN ), has a nominal value of 3.0V but a minimum and maximum range of 2.5V to 3.2V per the data sheet. I can't find any information in the data sheet that indicates the cause…
Other Parts Discussed in Thread: ADS1606 , OMAP-L138 I have a tmdxoskl138 EVM which is the L138/C6748 development kit that I would like to test the ads1606 evm with. Does the 5-6K interface module allow me to connect the two evm modules together?
Hi Simone,
Pins 5/6 of J4/P4 are technically shorted together through R34, so it really should not matter. By the schematic at the back of the Users Guide, pin 6 is AGND so we'll take a look into Table 3-1. For the reference, by the schematic on pg…