Other Parts Discussed in Thread: ADS4149 , ADS5281 Hi
I am looking for the vhdl/verilog code of the TSW1200, can you send me a copy? My email is jothiadithya@gmail.com
Jothi
Other Parts Discussed in Thread: ADS5281 Hello,
I wanted to convert the LVDS ouput of ADS5281 to LVTTL/cmos .So I decided to go with high speed differential line receivers..
But speed of ADS5281 which i am going to use in my project 50 Msps 12bits/pulse…
Other Parts Discussed in Thread: ADS5281 hello sir,
Can anyone help on this one ? I will be very happy ...In the below figure ADS5281...till some point ADC is not ready for data conversion ..it is taking some sample of clocks to make device ready and initialization…
Tariq,
I'm not sure the OMAP uPP can handle the data from 6 ADCs across its parallel interface. You might need to use an FPGA to handle it first. If you move to an FPGA, consider a serial LVDS 12-bit, 8-channel like ADS5281.
http://www.ti.com/product…
Other Parts Discussed in Thread: AFE7225 , DAC3484 , DAC5687 , DAC38J84 , ADS5281 , ADS5281EVM , DAC3482 , AFE5808A Dear all,
For my Master's Thesis, I have an experiment setup, where I need a sine generator of up to 2 MHz, an 8 channel ADC with 20 Msps and some…
Other Parts Discussed in Thread: ADS5281 Here I have a question regarding ADS5281 ....
here output of converter system clock , frame clock (ADclk and Lclk) and output data can we make dem in phase? yeah i have seen the data sheet it says we can program…
Hi,
Since that device you call out is only two-channel, you would not be able to fit all 10 of the LVDS signals from an ADS5281 into one buffer device adn so you would have to be converned with the 400ps part-to-part skew. If you used a buffer that was…
Hi Christian , thanks for your quick reply !
I'm considering one of the following : ADS5281, ADS5282, ADS5287, ADS5295, ADS5292 or ADS5294 .
But does the TSW1400 card include signal conditioning ?
For example, i see that the ADS5287 has a Analog Voltage…
Toshio-san,
From the previous posts:
1. Output Impedance=1ohm
2. CW Output Impedance=50kohms
3. I agree that the drawing is correct and the differential output impedance would be 2ohms.
Page 29 of the datasheet gives some good information about interfacing…