Hi Richard,
Attached is the screenshot. You can see it shows as USB Serial Converter
I tried with 2 ADS5282EVM and both show the same thing.
One more thing about the setting: I just applied +5V at JI and it's return to J2.
Thanks.
BAS
Hi Richard,
Thank you for your information. Can you tell me some of the TI ADC EVMs which can measure the signal from DC to 20 MHz or higher. I need 4 ch, 12 bit+ ADC EVM and used for ML605 FMC with an adapter card. If I am right, the output should be…
HI Richard,
Can you please send me the source code that you use for interfacing the DAC34H84EVM and ADS5282EVM? I will be using the ML605 for that. From your point of view, do I need to change anything else then the constraint files and all the IDELAY…
Mukul,
Problem with MityDSP board is that there is no direct interface to interface LVDS A/D converter for example, ADS5282EVM.
What are other possible ways to transfer data from FPGA to OMAPL138 with that high data rates ? Is it possible to do that using…
Other Parts Discussed in Thread: HSADC-SPI-UTILITY , ADS5282 , ADS5282EVM Hi,
I recently got the ADS5282 EVM without the CD. I downloaded the ADC SPI software from: http://www.ti.com/tool/hsadc-spi-utility
But instead of installing the TI ADC SPI interface…
Other Parts Discussed in Thread: ADS5282EVM Hi,
I want to clock data from ADS5282EVM to FPGA 3a DSP 3400 via FMC interface.
At this time i am using a DCM to produce two clocks (CLK0, CLK180), in order to clock the IDDR2 cell.
When i observe signals…
Other Parts Discussed in Thread: ADS5282EVM , ADS4146 , ADS5282 I am evaluating ADS5282EVM and Xilinx SP605 (Spartan 6 FPGA) boards.
Can I ask you to send me verilog code for TSW1200EVM
My e-mail: gruzinsky@pnpi.spb.ru
Regards,
Nikolay
Other Parts Discussed in Thread: ADS5282EVM Greetings to all
I have purchased the ADS5282EVM ADCs which are programmed by an application which functions on Windows.Currently I wish to develop a data analysis application on Linux (64bit) without having…
Thanks, Richard.
But when I probed the user guides of AFE5851EVM & ADS5282EVM, it appeared to me that the connectors from them are *not* identical. The connector from ADS5282EVM is similar to the connector in the FMC-ADC adapter, whereas that of…
Other Parts Discussed in Thread: ADS5282EVM , CDCE72010 , ADS5282 Hello,
I have ADS5282EVM. I succesfully connected to spartan 6 sp601 via FMC to ADC adapter.
I would like to clock the ADS5282EVM using spartan6 clock resources and not a function generator…