Part Number: ADS5421 Tool/software: Hi,
ADS5421 sample rate range from 1MHz ~ 40MHz, I want to know the tracking phase duration time is fixed or variable following sample rate.
If it work at fixed tracking phase duration time, then how many nano-second…
Part Number: ADS5421 Is it possible that instead of powering up supplies in a sequence if we keep the ADC in power down mode during power up without following particular sequence and than release the power down pin
Part Number: ADS5421 Hello,
I'm driving the analog input signal beyond the reference rail of the ADS5421. My reference voltages are as follows:
VREFT = 3.5V (Externally driven with unbuffered series reference)
VREFB = 1.5V (Externally driven…
i have two ADC'S in a board one is having CMOS25 standard (ads5421) other one has serial LVDS outputs. both are feeding the common FPGA but not simultaneously so i wanted to shift the fpga input pins from LVDS section to CMOS Section like a SPDT bus for…
Other Parts Discussed in Thread: ADS5421 hello ,I want to buy a C6455 DSK、a ADS5421 EVM,and a 5-6K interface board to connect the output of ADS5421 to the EMIF interface of C6455,now there are two questions:
a) I don't konw whether these three boards…
Couple of quick things Akash,
1. Where is your DC bias current path for the V+ inputs to the op amps?
2. This differential I/O op amp circuit sometimes has a common mode oscillation - probably not here, but we did see that in the OPA838 decomp device…