Other Parts Discussed in Thread: ADS5560 , THS4502 , CDCE72010 Hi
I'm trying to use the ADC ads5560 with my own PCB , but I'm having some problems .
I am connecting the ADC with an FPGA that is also responsible for generating the clock . When the clock is generated , the…
Other Parts Discussed in Thread: ADS5560 , ADS6149 Hello,
Is there a Matlab interface for the TSW1200 and ADS5560? Does this interface give me more options and control over the ADC then with the TSW1200 interface? I have also noticed that the TSW1200 interface…
Marcel,
Follow the attached instructions to program this EEPROM but use the ADS5560.xml file attached instead of the one called out in the instructions.
Regards,
Jim
ADS5560.xml
<?xml version="1.0" encoding="utf-16"?>
<FT_EEPROM>
<Chip_Details…
Other Parts Discussed in Thread: ADS5560 Hello Engineers,
Using the ADS5560 EVM, I am trying to reproduce the results shown on page 27 of the datasheet for the ADS5560 chip. The image below shows the output spectrum I generated with a 2 MHz input tone…
Other Parts Discussed in Thread: ADS5560 , CDCE72010 hi,
In the current project, we use ADS5560 whos sampling rate is 30.72MHz, and the sampled data is transferred to Spartan6 through DDR LVDS parallel port.
the sample clock signal into ADS5560 is generated…
Other Parts Discussed in Thread: ADS5560 To one who may concern :
We are using the ADS5560 in our project.
We are having problem with outputs, inclding CLKOUTP, CLKOUTM, and D_P & D_M alway in tri-stated mode.
We tried all kind of reset (hard and…
Other Parts Discussed in Thread: CDCE72010 , ADS5560 Dear community,
I was planning to use CDCE72010 to provide CLK for ADS5560, but there are still some questions make me confused.
e.g.1 ADS5560 is supposed to work at the sampling rate of 40MSPS and…
Other Parts Discussed in Thread: ADS5560 Dear engineers,
After I have read up the datasheet of ADS5560, I found that the number of FFT points was not given in the part of typical characteristics. Take figure 26 for example, I can't obtain the number of…
No ADC with quite that high of an input signal capability, but check out the ADS5560 (16-bit, 40 MSPS). It supports up to 3.6 Vpp full scale input signal.
--RJH
Hi Mukul,
Thank you a lot for your response.
I have considered DAC34SH84 and ADS5560 convertors so far. Do you think that they could be used with TMS320C6748?
Additionally, do you think that for my application some other DSP could be maybe more suitable…