Part Number: ADS5562 Other Parts Discussed in Thread: TINA-TI , , ADS5560 Tool/software: TINA-TI or Spice Models Hi,
I've looked everywhere and was not able to find a spice model/netlist for the ADS5562. Is there a reason why its only available in IBIS…
Part Number: LAUNCHXL-F28377S I have a Launchxl-F28377S but it seems not suitable to my application and I wonder which microcontroller is suitable to this application? It is not easier to figure out one in C2000 family.
The application:
Impedance mea…
Part Number: ADS5560EVM Other Parts Discussed in Thread: TIDA-00069 , ADS5560 , ADS4249 Dear TI expert,
I am looking for an evaluation platform for ADS5560EVM, in TI's document, it mentioned " High Speed ADC to FMC (Xilinx) Header Adapter Card " and…
Other Parts Discussed in Thread: ADS1602 , ADS5560 , ADS5562 , ADS1605 Hi.
I want convert a signal with 1000hz frequency and rise time 100ns .
can i convert this signal with ads1602?
thanks
Part Number: ADS5562EVM Other Parts Discussed in Thread: ADS5560 , ADS5562 Hello,
I'm using a TSW1400EVM module with the ADS5562EVM with HSDC Pro v4.50. According to the documentation the default jumper settings on both boards allow for data capture using…
There are couple of options to look at:ADS5481 16-bit 80 MSPS
ADS5560 16-bit 40 MSPS
Both options yield good SNR performance above 80 dBFS and good SFDR performance better than 90 dBc. The ’81 has higher power consumption…
Other Parts Discussed in Thread: ADS5560 I need to design an interface to a (newly ordered) ADS5560 EMV having CMOS data output, but the schematic supplied from User's Guide SLAU260-December 2008 only shows 14-bits available on output connector J5. A…
Other Parts Discussed in Thread: ADS4145 , ADS4142 , ADC16V130 , ADS5560 Hello,
Are there any app notes on interfacing the ADS4142/ADS4145 to the RF LNA buffer? This is the software defined MP01-HF radio. Also, is a 16 bit ADC version planned for this low…