Part Number: ADS6142
Hi, Could you tell me about the ADS6142 PDN pin processing. Should I PDN pin be open processing when using serial communication? Please tell me recommended processing. Best Regards, Yusuke/Japan Disty
Part Number: ADS6142 Hi Team,
Please advise me questions bellow:
Q1. The ADS6142 has OVR pin when it is configured in CMOS mode. Does this pin has open collector type driver or push-pull type driver?
Q2. Is the OVR positive logic or negative logic…
Hello,
ADS6142-HT SLWS234 - December 2011 Datasheet has bond pad numbers 47, 50, 55, 56, 61, 64, 67, 70 and 72 with a description of SUBST. The backside potential is listed as DRVSS. Should the SUBST bond pads be connected to DRVSS along with the backside…
This is a 65Msps device, but the curves in the datasheet (Figure 29) go to 125Msps. My customer would like to know if the device will operate to 125Msps, with the understanding that the performance will be degraded.
Part Number: 66AK2G12 Other Parts Discussed in Thread: ADS6142 Hi,
Today we use analog converted ADS6142 and the DSP TMS320C6746EZCEA3.
The ADC is sampling 10Mhz signal and have parallel output. The DSP has uPP block which is parallel port that fits…
Dear Tom,
Thank you for reply. We have used ADS6142 in our old design,this part was used for -1V to 1V input signal range. Now requirement is input signal range 0 to 2V . Now we can go to any other new part. My doubt is any ADC which supports 2Vp-p…
Hi,
I am not familiar with the pinout of a Microsemi FPGA board, but if it is FMC then i would suggest checking to see if they followed the same pin assignment as Xilinx used, as we do have the adapter board to adapt from our EVM connector to the FMC…
Hi,
What is IHM? I don't recognize that acronym. You are looking at the FFT or the time domain data on HSDCPro?
I think I need to make a new device ini file for you to add to the HSDCPro installation. You are using the device selection ADS614x? That…
Other Parts Discussed in Thread: ADS6143 , ADS6142 , ADS6144 Hi, Could somebody answer my question, please. Is there any way to digitize a signal with the bandwidth 10 MHz (single channel) directly at IF, which is 70 MHz for further processing in DSP…
Other Parts Discussed in Thread: TMS320F28335 , ADS62P42 , OMAP-L138 , ADS6142 Hi,
Currently I have the TMS320F28335 experimenters kit. However, my program is getting larger and I would need more memory. I use the 32 KB RAM memory available in the linker…