Hi Evan,
It turns out I can't configure the SPI interface on the BB Black as a slave.
If I use two of the ADS7054 instead ( www.ti.com/.../ads7054.pdf) do you think it'd be better to configure it like the below picture, where I have the BB Black SPI…
Hi Biser,
In that case, is it a plausible solution to have both SPI interfaces on the BB Black act as masters, and have SCLK on SPI0 and SCLK on SPI1 provide separate, 24 MHz clock signals to SCLK on two ADCs (ADS7054) like in the below picture?
Regards…
Part Number: REF2030 Other Parts Discussed in Thread: ADS7057 Hi,
I plan to use 5 ADS7057 ADC simultaneously. I supply the AVDD rails using a REF2030 voltage reference with 20mA source current capability. The REF2030 maximum recommended output capacitor…