Other Parts Discussed in Thread: ADS7863A Hallo,
Can the ADS7863A be used in the input range of 0V to 5V? Looking at Table 9 of the datasheet, it seems that the input full-scale range of CHxx+ is 5V when CHxx– = VREF = 2.5 V, and the output ‘7FF’ will…
Question reg app note SLAA597 - Intro to ADS7863A. My design already in production uses ADS7863, Mode I, RD pulse 2 clocks wide.
According to P.2, Table 3 in the app note, The RD width can be up to 16 clocks, but in P.3, Figure 1, the max hold time for…
Hello,
The ADS8558 is only a 730kSPS sampling rate device.
Would you provide more detail as to what are some other requirements for the device? the ADS8558 is a multi channel simultaneous device, to find a multiple channel device that can reach 2MSPS will…
Hello,
I did a quick parametric search based on some assumed key parameters, and found 8 devices - click here- that could fit this
Specifically I would suggest the ADS7863A or the ADS7869 . both these devices seem to be appropriate alternatives.
Regard…
Part Number: AM6548 Other Parts Discussed in Thread: TIDA-01555 , ADS8598H , AM2634 Hi
I'm new to processor with PRU as well as real time micro-controllers. I have a requirement to sample 5 channels simultaneously with maximum sampling rate possible. …
Hello RJH,
RJH_A> You may be able to and your MCU interface may dictate a Precision ADC.
I 'm change Precision ADC device the perspective direction.
I searched for Ti devices(Precision ADC).
1. ADS7863A 4Ch, 2000kSPS, 12bit , SPI , SAR
2. TH…