Part Number: ADS7924 In the abs max table of the datasheet, the abs max is listed as 300mV.
Should this be ADD + 300mV instead?
It appears the input shave both GND and VDD diodes, correct?
In addition, any risk in have bias applied to input pins…
Part Number: ADS7924 Other Parts Discussed in Thread: TLV9004 Hi,
Does anyone know the impedance for the analogue inputs on the ADS7924? I can't see it in the data sheet, but that may just be my bad eyesight!
Thank you
Part Number: ADS7924 Other Parts Discussed in Thread: ADS8332 Hi,
I am looking for the timing requirements for a reset pulse using the external reset pin on ADS7924. I can not see this information listed in the datasheet.
Thanks
Simon
Part Number: ADS7924 What are the timing requirements for the software reset on the ADS7924? It doesn't appear to be mentioned anywhere in the datasheet (similar vein to e2e.ti.com/.../755048).
I've placed a 100uS delay between sending the software…
Part Number: ADS7924 Other Parts Discussed in Thread: ADS7828 Hi Team,
Do you have a linux driver for ADS7924? Or any simple code or reference code could be shared to drive ADS7924 through linux for my customer?
Best regards,
Albert Lee.
Part Number: ADS7924 Dear Team,
My customer is considering to add an OpAmp between MUXOUT and ADCIN of ADS7924 to improve sensing performance. The ADS7924 datasheet describes about the RC filter setting at "8.1.2 Using an Operational Amplifier and…
Hi Rene,
I sense your frustration and I apologize for my quick response without taking a closer look at the logic analyzer shots with a tool I'm unfamiliar seeing.
When I have used the ADS7924 in the past, I always set the device to Awake in the…
Part Number: ADS7924 I do feel a bit stupid as I fail to write/read the registers of the ADS7924.
What I do:
1. check whether the ADS7924 is present by simply writing the address and checking whether it is acknowledged - which works.
2. resetting…