Part Number: ADS8166 Hello,
I am having trouble reading proper data from the ADS8166. We have configured the module with the following: - External 5 V reference.
- Deactivated the internal reference, refby2 and buffer.
- We are outputting the data + channel…
Part Number: ADS8166 Hello,
My customer is interested in using ADS8166 with DVDD = 1.8V, however, the device states that it's specified DVDD is from 2.35V to 5.5V (3V typical) even though it's operating DVDD is from 1.65V to 5.5V (3V typical).…
Part Number: ADS8166 Hi Folks,
The ADS8166’s SPI interface can operate @ 70MHz. The period of the clock cycle @ 70 MHz (~14.3 ns) is shorter than the 19ns (max) for the SDO delay (td_CKDO) from rising clock edge. So the delay could be 1-whole clock-cycle…
Part Number: ADS8166 Hello,
The td_CKDO of the ADS8166 (19ns maximum) is not compatible with our master SPI that specifies a MISO Data Hold after SCK Rise of 40ns minimum.
Is there a configuration that can remove the early data launch of the ADS8166 SDO…
Part Number: ADS8166 Hello ,
We are using the auto sequence feature of the ADS8166 following the steps on page 34 of the datasheet to mimic figure 48. But after we issue the start command our SEQSTS pin never goes high. I see a note in SDO_CNTL4 that…
Part Number: ADS8166 Other Parts Discussed in Thread: ADS8688A , ADS7066 Hi team,
Could you tell information about DIGITAL INPUT/OUTPUT of ADS8166?
The picture below is the example of ADS8688A.
Regards,
Noriyuki Takahashi
Part Number: ADS8166 I am currently using the ADS8166 ALERT feature. where I am able to trigger an ALERT pin using HI_THRESHOLD, but that pin not automatically pull down when my voltage is below HI_THRESHOLD.