Other Parts Discussed in Thread: TMS320F28335 , ADS8328 , TEST2 I have an ADS8328 hooked up to the McBSP of my TMS320F28335 and am using it to read in from two different audio sources. I have designed a small library that initializes the device into Manual…
Other Parts Discussed in Thread: ADS8328 Hello,
What should I do with the CONVST pin if I intend to use the ADS8328 in auto mode? Should I tie it low, high or leave it floating?
Could you please update the data sheet with this information as well for other…
Other Parts Discussed in Thread: ADS8328 Hi, I'm a student trying to program an ADS8328 but I've had a little problem interpreting the datasheet.
Table 4, on page 30 of the datasheet, has a list of serial commands. However, I am unsure when the…
Other Parts Discussed in Thread: ADS8328 Hi,
I am trying to interface the Ti ADS8328 with the C5515 ezDSP board. I trying to set SPI_CS1 to be active low , but the CS1 line keep high 3.3V.
anyone can help why SPI_CS1 keep mode HIGH and not set to LOW 1…
Other Parts Discussed in Thread: ADS8328 Hello.
How to code to write or read CFR of ADS8328?
reset = WRITE_CFR |
!AUTO_CHAN|CCLK_INT|MAN_TRG|D8_DNC|
!POL_INT_EOC_LOW|PIN10_EOC|PIN10_OUTPUT|ANAP_DISABLE|
RESUME_NAP|RESUME_DEEP|!TAG|!NO_RESET;
SpibRegs…
Other Parts Discussed in Thread: ADS8328 Hi everyone,
I am an absolute beginner with the TI DSP programming and the CCS. I would really appreciate if someone can help me a bit. I have the Pulse Oximeter Front End Board along with C5515 EVM. I know the…
Other Parts Discussed in Thread: ADS8328 Friends,
I designed the ADS8328 into an unattended field recorder product several years ago. I worked around its quirks and have built over a 60 units but have never seen this event. Unfortunately all I have to…
Other Parts Discussed in Thread: ADS8328 Hi,
I am working with the ADS8328 and I have a couple questions with having the following settings:
VA = 5 V, VBD = 3.3 V, REF+ = 4.5 V
What is the impact of using a REF+ slightly higher than the rated max of 4.2…
Other Parts Discussed in Thread: ADS8328 , REF3325 , TL431 I HAVE CONFIGURED ADS8328 IN
1)MANUAL CHANNEL SELECTION . 2) TRIGGER SELECT - MANUAL.
I HAVE SELECTED ONLY CH0.
VREF TO ADC8328. IS 2.5V.
I AM GIVING ANALOG INPUT (0V TO 2.5V) THROUGH AGILENT MULTIFUNCTION…