Other Parts Discussed in Thread: ADS8361EVM , ADS8361 I'm puzzled with interfacing the ADS8361EVM (evaluation board for ADC ADS8361) with an arduino (Mega) via SPI.
Is there a sample code (alternatively in C or any other language) for reading the channels…
Other Parts Discussed in Thread: ADS8361EVM , ADS8361 , 5-6KINTERFACE Dear all
I would like to eventually incorporate one of TI hi precision A-D's into a general A-D board, and wanted to start using the ads8361evm board - could I
just clarify the…
Hello Shshan,
Sushant Kamble said: We taken 60000 samples with 10 KHz and SPI Speed is 2 MHz.
what is the amplitude of this signal? does it also have a common mode of 2.5V? Could you share how this looks like on an oscilloscope
Sushant Kamble…
Hi Walsh,
The schematic shows that you are using an ext reference REF5025.
The REFOUT pin is the output of the buffered internal reference, and I suspect that connecting this pin to GND may be causing an issue.
Looking at the ADS8361EVM evaluation…
Other Parts Discussed in Thread: ADS8361EVM Hi, I'm working to setup a test bench with some EVMs 6418EVM, which should be compatible with 5-6k interface board. I need help for some informations about ADC/DAC EVM compatibility because sometimes is it not…
Other Parts Discussed in Thread: ADS8556 , ADS8361EVM , DAC8831EVM Hi,
I planned to plug in an ADS8556 EVM AND a DAC7741EVM TOGETHER onto a 5-6K interface board, which was to be connected to a C6713 DSK. Since both the EVMs are parallel they did NOT…
Other Parts Discussed in Thread: ADS8361EVM , ADS8361 , ADS8363 , ADS8363EVM , DAC8831 Hi,
I am working on a concept system composed by 6418EVM and 5k-6k adapter board with 1 DAC8331 EVM and 1 ADS8361EVM, each connected to one of the two McBSP interfaces…
Hi Umar,
I believe both the DAPSIGCNDBRDUNPEVM and DAPSIGCNDBRDBPEVM bring the common mode up to +2.5 so a bipolar +/-2.5 or single supply 0-5V signal would be accommodated by the ADS8361EVM. You can change the gain on either board to take your +/-10…
Hi Basu,
The ADS8345 can run at 100ksps single channel, 50ksps two channels, 25ksps four channels, etc. Both the ADS8361EVM and the ADS8345EVM are compatible with the 5-6K Interface card as is the DAC8814EVM. You will have access to two serial ports…
Other Parts Discussed in Thread: ADS8361 Hi, I'm planning to use ADS8361 for a 4 channel FSK-FH decoder, using 6418EVM, 5-6k interface board and ADS8361EVM .
I want to use mode IV operation of ADS8361 , and have the 4 channels 16 bit samples written…