Part Number: AM5748 Other Parts Discussed in Thread: ADS8598H I intend to use AM5748 based SoM for a data acquisition and control system.
My primary requirement is to acquire data from a high speed 24 bit ADC ( 4x4ch = total 16 channels) at an interval…
Thanks for your comments!
We have recently procure ADS8598H ICs & its evaluation board for testing. We would like to capture and do electrical signature analysis for 100th harmonics of 60-Hz 3-phase power lines, hence the required bandwidth would be…
Hello Sahil,
We have a few options for ADCs with digitally-adjustable input ranges
If you need all channels to be simultaneously sampled we have the
ADS9813 - for simultaneous sampling with 18-bit, 2MSPS and input ranges of: ±12V, ±10V, ±7V…
Hi Dale,
Thanks for your comments!
We have tested it again with ADALM2000 signal generator using 10Vp-p Sinewave of different frequencies up to 9KHz with -0.5dBFS amplitude which prevent clipping and getting better dynamic parameters of ADC. The test…
Part Number: ADS8598S Other Parts Discussed in Thread: ADS8598H This part supports Oversampling modes through pins OS0 OS1 and OS2. The datasheet states that the oversample is accomplished by taking multiple samples and averaging them together.
But…
Part Number: PROCESSOR-SDK-AM64X Other Parts Discussed in Thread: SYSCONFIG , ADC-PHI-PRU-EVM , ADS8598H Working with v08.06.00.45, I'm running into the following problem building a default example:
user@ubuntu:~/ti/mcu_plus_sdk_am64x_08_06_00_45$ make…
Hello KJ,
Welcome to E2E forum.
The conversion time(tCONV) on ADS8598S is related to OSR configuration, ADS8698S datasheet has specified this specification in 6.15 session(Switching Characteristics) on page 12.
OSR= 111 is an invalid configuration…
Hello Gareth,
Yes, if you follow this reference document the image you shared from ( Circuit to increase input range on an integrated analog front end (AFE) SAR ADC ) it goes through some of the calculations of how those components were selected.…
Part Number: AM6548 Other Parts Discussed in Thread: TIDA-01555 , ADS8598H , AM2634 Hi
I'm new to processor with PRU as well as real time micro-controllers. I have a requirement to sample 5 channels simultaneously with maximum sampling rate possible…
Hi Kazuya,
The voltage reference's output voltage accuracy, temp drift and noise definitely can affect your conversion accuracy, however the amplitude of reference voltage does not improve your accuracy, actually f or low resolution (16-bit) ADCs where…