The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: ADS9813 Tool/software: hi Sir
I use the ADS9813 in our project, but next project need the 20bit
did you have a solution like as the ADI/AD4856
thanks
AD4856 Datasheet and Product Info | Analog Devices
Part Number: ADS9813
Tool/software:
ADS9813 ADC can transfer data over the SPI at high speed to MCU?
Our usage sampling rate is 1MSPS only. So is it possible to data transfer through SPI?
If it's not possible then can we use/interface DCKOUT, FCLKOUT…
Part Number: ADS9813 Tool/software: hi:
The datasheet of the ADS9813 states that the sampling clock input range is 3.1-8.1 MHz. How does this correspond to achieving a 2 MHz sampling rate for 8 ADCs? If we require an effective sampling rate of 0.8 MHz…
Part Number: ADS9813EVM Other Parts Discussed in Thread: ADS9813
Tool/software:
Hello,
We are using the ADS9813 EVM along with the Zynq 7045 FPGA. The ADS9813 is mounted on the FMC of the FPGA. We plan to use the ADS9813 in a 4-lane SDR data rate configuration…
Part Number: ADS9813 Tool/software: Can differential inputs be as low as ~ +/- 20 mV, or should these signals be amplified (how much) before ADC (ADS9813)?
Part Number: ADS9813 Team, I saw that we provide IBIS model for ADS981x on TI.COM. But do we have some behavioral models (like Verilog or VHDL) for the ADS981x digital interface that we can share? This is to help for FPGA side IP development to interface…
Other Parts Discussed in Thread: ADS9813 , ADS9811 , ADS9817 I would like to get the finalized datasheet for ADS9813 / ADS9811, as the prelim datasheet didnt show up the package/mechanical/dimension information. Understand that this is a new product, please…
Hi Rick,
Thanks for your post! Out of curiosity, do you need the full 8MSPS/CH sampling speed to measure your load cells? Are you only measuring two voltage signals? We do have a slower, higher channel count ADC: ADS9813 - 18-bit, 8CH, 2MSPS/CH ADC. There…