Part Number: AFE7900EVM Hi! Please direct me to the latest code and guidance docs to get AFE7900EVM up and running with AMD ZCU102. Thanks! We will use the Simulink model in the secure folder to get more familiar with this part family - looks useful.…
Part Number: AFE7900EVM Hi,
I'm using the Latte Scripts to configure the AFE7900EVM, and I'm running into an issue where only Channel A responds to configuration — the remaining channels (B, C, D, etc.) do not appear to be configurable / do not reflect…
Part Number: AFE7900EVM When using the AFE7900EVM and LATTE GUI to set the FADC sampling rate to 2560MHz, setting the following frequencies to the RX Center Frequency (NCO) causes setting errors and prevents data capture. I'm using RXB. 1)There's a setup…
Part Number: AFE7900EVM Other Parts Discussed in Thread: AFE7950 Hi,
I want to obtain DAC output from all four TX channels simultaneously, but the board only outputs on max two channels.
Setup:
The AFE7900EVM is connected to an Avnet UltraZed-EV…
Part Number: AFE7900EVM Other Parts Discussed in Thread: AFE7950 Hi,
We would like to validate the AFE7900EVM board with our custom board. Could you please provide any available drivers or bare-metal example code to support this?
Thank you.
Part Number: AFE7900EVM Other Parts Discussed in Thread: AFE7900 I am using an AFE7900EVM board, connected to a ZCU102 Evaluation platform. When I received the boards, I went through the reference design and setup using Latte and Vivado. I was able to…
Part Number: AFE7900EVM
Hello, I am trying to work with 2 lanes on TI_204c_IP. My current configuration is like this:
// The following parameter defines if the
// IP is in 8b/10b mode or 64b/66b mode
// Leave the second line commented if it is
/…
Part Number: AFE7900EVM I am working with the AFE7900EVM and want to design a custom AMD FPGA design with it. I got access to the TI-204C JESD204 rapid design IP site but the license agreement seems prohibitive espessially section 5 I pasted below. Is…
Part Number: AFE7900EVM In Latte v2.5.0 (Latte framework 5.7.3), after having done saveSystemParamsJson(..) and reloading it with loadSystemParamsJson(..) [both fns defined in mAfeBaseClass.py], sysParams.gpio_mapping dictionary contains entries such…
Part Number: AFE7900EVM Tool/software: We require updated app note for interfacing ZCU102 with AFE7900EVM and procedure document with required files for integrating through SPI as the mentioned TI SPI IP which is mentioned in bring up guide is not available…