Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG , Hi,
The latest AM13E23019 datasheet changed the CPU clock frequency specification to 250MHz. Is it possible to configure the sysconfig of one of the AM13E23019 SDK examples to increase…
Part Number: AM13E23019 I want to use bankswapping as discussed in TRM 3.5.2.1.2 and 13.6.1.
Can someone find/provide the following for AM13E23019. A bit-field figure, a header fragment, or an errata/addendum to Table 3-27 are all sufficient.
FLBANKSWAP…
Part Number: AM13E23019 Hi Expert
This is not the question, share the EPI code execution demo: epi_sdram_read_write_am13e230x_som_m33_nortos_ti_arm_clang.zip
Supported by 26.01.00 SDK release
Thanks
Joe
Part Number: AM13E23019
Hi, While using CCS 21.0.1 and AM13E2X SDK 26.01.00.03 , If we try to run the example: am13e230x_sdk_26_01_00_03\examples\driverlib\epi\epi_sdram_read_write and see the register values at address 0x4001A000 onwards in the memory…
Part Number: AM13E23019 Hi,
How do I create a static library for AM13E23019 using CCS 20+? Are there any template projects available?
If this feature is not currently available in CCS, are there plans to integrate it in the future?
Ari
Part Number: AM13E23019 Other Parts Discussed in Thread: DRV8323 Hi,
The AM13E23019 SDK has an example project, "1sh_sl_foc_drv8329a", which demonstrates allocating a function in SRAM. This function is called from an ISR, but the ISR is allocated in…
Part Number: AM13E23019 After performing the 64 bit write operation we would like to verify the first programmed byte for containing the correct data, however, when checking said byte, the value that is obtained via read would appear to be 0xFF when the…
Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG Hi,
How to create a new project for the AM13E23019 so that all dependencies are in the same folder. This way, when copying the project folder to another computer, the project can be…
Part Number: AM13E23019 Other Parts Discussed in Thread: SYSCONFIG Hello TI Experts,
I am experiencing a JTAG debugging issue with the AM13E23019 MCU on our newly assembled custom boards. Out of 4 boards tested, 2 boards work fine, but the other 2 boards…