Part Number: AM1808 In AM1808, I have a 3.3V power line with about 1.4V left in it even though I have power-off. AM1808 has provisions for power-on, but no detailed provisions for power-off. Is there a correct sequence of power lines to power-off?
…
Part Number: AM1808 Hello
I got the latest am1808 sdk Linux from TI version 606.0
Linux EZ SDK for AM1808, AM1806, AM1802
I found u-boot-2010.12-psp03.21.00.04.sdk in folder board-support
using
arm-linux-gnueabihf-gcc (Linaro GCC 5.3-2016.02…
Part Number: AM1808 Other Parts Discussed in Thread: SEGGER Hello,
I am trying to debug AM1808 with SEGGER J-Link and CCS8. But I have probrem to set up the CCS project. Could you help me?
I opened ccxml file on CCS, and chose "SEGGER J-Link Emulator…
Part Number: AM1808 Other Parts Discussed in Thread: OMAP-L138 , Hello ,
I'm using the OMAP-L138 am1808 base our custom board.
we have two usb port. as per our requirement we need internet connectivity using usb to Ethernet adapter.
we added support…
Part Number: AM1808 Hello Gentle Men
I'm still strugling with UART boot on BBone Blk brd
I failed to do on Linx using SX utility
AS unable to see any response on Linx
So I'm try Tera Term on Win 7 as described below
First Open with 1156200 8bit…
Part Number: AM1808 Other Parts Discussed in Thread: OMAPL138 hi Teams:
Customers want to use am1808 to make products. If they want to test with EVM and demo, where are the EVM and demo programs of am1808.
Part Number: AM1808 Hi Team,
My customer is use the VS2005 develop and enter debug simulation , but he found that if the red area is operated with 32MB, a memory error message will be generated(Even if the program memory (total) is set to 62MB, it cannot…
Part Number: AM1808 Hi team,
Customer want to konw 1.2V and 1.8V. Customer can find "AM18x Power Spreadsheet", but they want to know the condtion.
Is total power for 1.2V and 1.8V each? if not, please let us know power consumption for each voltage…
Part Number: AM1808 Our customer would like to use PI0 and SPI1, UART0 to UART2, I2C0, RMII on AM1808.(Please refer to Pin set up) When they set MDIO CLK and MDIO D of RMII, Chip Select 0 (SPI0_SCS0) and Chip Select 1 (SPI0_SCS1) cannot be selected in…
Part Number: AM1808 1.On my board, AM1808 I2C0 chain has 7 devices, and the test finds that the start position of SCL/SDA rising edge oscillates , as shown in Figure 1.
2.Then, I made I2C0 only direct to one slice EEPROM by flying lines and found…