Part Number: LP-AM243 Tool/software: I would like an easier method than described here:
LP-AM243: [LP-AM243] AM2434 Firmware Upgrade Over Ethernet - Need Follow-up
Also we need to avoid the Errata Item i2331 issue.
Our board, yet to be designed…
Part Number: AM2431 Hi Team
We are using AM2431 in our design, we have shortlisted the PSRAMs with both 3.3V and 1.8V supply voltage to interface with the MCU. During the Noise margin analysis we came to know that all those PSRAMs are failing since…
Part Number: AM2431 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi
I want to change the clock frequency of my EQEP0 module. i noticed the code in the generated files by the sysconfig:
and afterwards it uses this structure to initialize…
Part Number: AM2431 Tool/software: Does the Texas Instrument FCCSP based package have an interposer between the silicon die and the solder bumps or are the solder bumps deposited directly onto the die itself? If an interposer is used, is it made of metal…
Part Number: AM2431 Other Parts Discussed in Thread: TMDS243EVM ,
Tool/software:
Hi, Experts.
Boot Mode is currently set on my custom board as follows.
BOOTMODE
0
1
2
3
4
5
6
7
8 …
Part Number: AM2431 Tool/software: I am using SDK8.3.0 (It is currently difficult for us to upgrade to the latest SDK version.)
I changed the definition of PBUF_POOL_SIZE from 30U to 50U in LWIP. I think the definition in the lwip2enet.h file will…
Part Number: AM2431 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Dear person in charge. We are developing a product using the AM2431, and the SDK version we are using is 8.03.00. We have incorporated the Enet LwIP CPSW example into our product…
Part Number: AM2431 Tool/software: Hi
After trying to import enet_cpsw_udpclient or enet_cpsw_tcpclient, CCS will have some errors. It seems that there is a problem with the project file link in the industrial sdk. Please help me find out how to fix…
Part Number: AM2431 Tool/software: I am using SDK8.3.0 (It is currently difficult for us to upgrade to the latest SDK version.)
I want to change the SO_SNDBUF, but it is not implemented.
I'd like to confirm that:
To achieve the functionality of…
Part Number: AM2431 Other Parts Discussed in Thread: UNIFLASH , Tool/software: Hi,
I have created a multicore project with a multicore payload that can be flashed into the AM2431. When flashed through UniFlash, it correctly flashes to the correct…