Part Number: AM2432 Other Parts Discussed in Thread: TPS65219 Hi,
I am looking for the power consumption of the AM2432BSDGHIALXR processor so I can properly spec the power supply circuitry for it.
The datasheet links to the AM64x/AM243x Power Estimation…
Part Number: AM2432
Hi all,
Sorry for reopening the ticket, but we have identified an issue during our cybersecurity testing activities.
Our cybersecurity lab observed that there may be vulnerabilities in the Texas Instruments EtherNet/IP stack…
Part Number: AM2432 Other Parts Discussed in Thread: TMDS243EVM Hi,
I am trying to configure GPMC on the tmds243evm into a multiplexed mode. I configured GPMC_CONFIG1 register with GPMC_CONFIG1_MUXADDDATA_MUX but after setting this bit, the AD lines…
Part Number: AM2432 DLR Ring Network Fault Report
1. Overview
The devices are based on the AM2432 and are networked in a DLR (Device Level Ring) topology. Under specific traffic conditions, the ring network malfunctions, exhibiting symptoms such as…
Part Number: AM2432 Hello, we are designing a single-port PROFINET IO RT device (Conformance Class A) for Siemens S7-1200/1500, 100–1,000 units/year, and are evaluating AM2432BKFGHIALXR (ALX package, "F" variant) with the AM243x Industrial Communications…
Part Number: AM2432 Hi TI experts,
Our environment is Omron NX502 PLC as the master station(sysmac ver 1.69), AM2432 device(Node 0x17) as one of the slave station via ethercat.
When establishing communication, the master station receive AL status…
Part Number: AM2432 Hello team,
In our application, we are using AM2432 controller in which we have to implement onewrie functionality. As per my knowledge, oneWire is fully software oriented functionality which can be implemented on general purpose…
Part Number: AM2432 Other Parts Discussed in Thread: AM2434 Hi TI Experts,
Customer has a new SST project that needs to run 3 Ethercat loops to control 3 phases separately. On each of the slave side of the corresponding phase, custoemer used F28P65…
Part Number: AM2432 Hi,
I am using AM2432 with the Industrial SDK 11.00.00.08.
I successfully converted a device from HS-FS to HS-FE using KeyWriter. Then I flashed the SBL and the application, both signed with my SMPK, and everything is working properly…
Part Number: AM2432 Hi,
I am using AM2432 with the Industrial SDK 11.00.00.08.
I am interested in using DKEK to encrypt data.
I'm reading here that there are two possible mechanisms, but I've had problems with both. Using the first mechanism to…