Part Number: AM2432 Tool/software: Hi
AM243 EVM PRU-ISCCG1 port are compliant with MII/RGMII. I want to check if customer develop AM243 as Ethercat slave, do they need to design the customer board that compliant with MII/RGMII at the same time? Or just…
Part Number: AM2432
Tool/software:
Hi,
I am using AM2432 with Profinet from the Industrial SDK 09.02.00.24.
Our team has performed a cybersecurity scan with the tool Nessus, and the two problems in the screen were found:
I already asked in my…
Part Number: AM2432 Tool/software: HI TI Extert,
Can you please check and confirm that 'AM2432BSEFHIALVR' operate/RUN without external flash memory?
-
Vaibhav
Part Number: AM2432 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi all,
I'm currently working on EtherCAT with AM2432 + DP83822 custom board.
Board configuration:
Port 1 -> PHY address 3
Port 2 -> PHY address 1
I got my EtherCAT…
Part Number: AM2432 Tool/software: Hi TI Experts,
Customer has a strange AM243 board that the Ethercat link status read out from the PHY (DP83822, addr: 0x0019) is different with the actual status.(all other boards are normal) For example, if the Ethercat…
Part Number: AM2432 Tool/software: Hey Ti,
We are using PRU stigma delta, trigger based, double update mode. When SD finishes, it generates an interrupt on ARM R5F side. We configured this interrupt (SD ISR) to highest priority. But we found the moment…
Part Number: AM2432 Tool/software: Hello Champs,
My customer is developing new secondary bootloader and its requirements is once it is power-up, it should enter second bootloader and start the CAN message TX within 450ms.
but when customer runs…
Part Number: AM2432 Tool/software: Hi, I understood that COL pin is needed for MII half-duplex when using ICSS Ethernet MAC and for full-duplex it is not needed.
When using full-duplex can the pin useed with other function as GPIO or should it be configured…
Part Number: AM2432 Tool/software: Hi TI
We want to use bcm89884 in our project which need clause-45 access method.
In EnetApp_waitForPhyAlive, we detected CPSW_MDIO_ALIVE_REG is 0x01, so our phy addres is 0.
Then we try to read phy register…
Part Number: AM2432 I would like to know if the pheripherals like PCIe drivers and APIs are available to use in NO-RTOS = baremetal case.
kindly provide related details by directling to suitable link.
Regards,
Amit