Part Number: AM2434 Hi TI,
On the AM2434 Sitara processor: Which polynomials does the PRU_ICSSG CRC16/32 accelerator support? Is the polynomial programmable?
Thanks,
Mohan
Part Number: AM2434 Hello TI,
On the AM2434 Sitara processor, regarding the the PCIe Gen2 x1 endpoint:
can an inbound address-translation entry target PRU_ICSSG0 shared RAM (and/or GPMC0 data space)?
If yes, which firewall/privilege settings must…
Part Number: AM2434 Hello Team Ti,
We have built a single protocol device(EthernetIP or EtherCAT). To connect to different PLC's in market we need one unit to be able to read EthernetIP in one Ethernet port and convert to EtherCAT on the other Ethernet…
Part Number: AM2434 Hi TI support,
How to use mcrc calculate a standard CRC32. For example, for calculating the CRC value of the 4-byte data 0xA5A5A5A5, and hoping to generate the result according to the standard shown in the figure below, how should…
Part Number: AM2434 Hi TI,
On the AM2434 Sitara processor: are bytes within one inbound posted-write PCIe Transmission Layer Packet (TLP) guaranteed to be written to the target in address order?
Thanks,
Mohan
Part Number: AM2434 Hi Team,
I am using AM2434 for developing EtherNET/IP adapter application on custom board.
I am using example project ind_comms_sdk_am243x_09_02_00_24\examples\industrial_comms\ethernetip_adapter_demo\profiles\generic_device\standard…
Part Number: AM2434 Hi,
I have questions regarding the startup sequence of the R5F clusters in the AM2434 EVM sbl_ospi boot flow.
Does SBL 'SelfCpu' refer only to R5FSS0_0, or does it refer to the entire self cluster 0 containing both R5FSS0_0 and…
Part Number: AM2434 Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH We are currently testing a DDR4 interface between an AM2434BSDFHIALVR and an ISSI IS46QR16256B-083RBLA2 memory at 800MHz, and after using the Sysconfig tool to generate a configuration…
Part Number: AM2434 Other Parts Discussed in Thread: SYSCONFIG Hello, TI support.
Question related to the PCIe initialization for AM2434.
Configuration is: AM2434 at custom board. Running as an EP at Linux machine. sysconfig 1.28.0 + sdk_12_00_00_27…
Part Number: AM2434 Hello,
I would like to use the ADC on the AM2434 to measure the current of a motor phase. I have designed the following circuit for this purpose:
As shown in the (simplified) circuit diagramm, the shunt resistor is not located…