Part Number: TDA4VM Other Parts Discussed in Thread: SYSBIOS Hi Experts:
the board is ourself, i build the psdk linux visions app,
pc connect tda4 board by 9G port
By default, 9g firmware is DHCP configuration, but I need to set the static address…
Dear Tanmay,
The SDK version is 6.3.0.106, below is dmesg log:
=~=~=~=~=~=~=~=~=~=~=~= MobaXterm log 2022.12.16 10:07:42 =~=~=~=~=~=~=~=~=~=~=~=
root@SunGrow:~# dmesg [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94…
Hi Krunal,
We used the latest 4KB version of the firmware and some other files, but there are still some issues. We recompiled the pvrsrvkm.ko according to the kernel with a page size of 4KB. When we run insmod pvrsrvkm.ko, the following log is printed…
Blake,
From the screen shot, it does appear that you have created the project with the Linaro compiler using Resource browser. Can you confirm that you followed the steps here while creating this example.
Using those steps, I was able to create…
Hi, to All!
I will try to describe our problems.
We have a custom board. DDR3 memory working fine. I have done all related DDR3 modification in u-boot and mtest don't show any errors.
We have 1GbE that is connected to the Marvell 88E1111 PHY with…
Other Parts Discussed in Thread: OMAP-L138
Hi everyone,
I got the ZOOM OMAP-L138 EVM DEVELOPMENT KIT and DaVinci-PSP-SDK-03.20.00.06 with Arago distribution developed by TI for OMAP processor.
I'm trying to communicate with an external spi device…
Part Number: DRA77P
Hi Team,
I am working on vision SDk v3.07.
I have implemented the single stage boot and have been loading the application apps.out through init-demo.sh
The following is the kernel command line I have used,
CONFIG_CMDLINE…
Other Parts Discussed in Thread: DRA821 , DRA829 HI TI !I
t is trying to boot by downloading the SDKLinux_08_00_00_05 version image from the evm board(DRA821,J7200). Kernel paic occurs while evm board is booting linux. The generated log is as follows…
Part Number: AM625
Dear Experts,
I have been actively involved in the development of a custom System on Module (SoM) across different processor SDK versions. In my previous inquiries , I encountered challenges related to the device tree source …
Hi
We want to integrate PVRSGX Graphics SDK with board similar to Centaurus (TI814x).
We are using Graphics_SDK_setuplinux_4_03_00_01.bin.
Our base kernel is 2.6.34.
As per the wiki pages available we were able integrate the file system changes…