Hi Bin, We wanted to try this working image on a Bigger NAND(BCH8) and are running into all sorts of problem....like NAND CRC errors and UBIFS errors... So I have stepped back and created a Tiny initramfs to try a working combination and have done uboot…
Part Number: AM3352 Other Parts Discussed in Thread: AM625 Tool/software: Hi Sitara support Team,
We are encountering issues with the RS485 reception on the AM3352.
Environment:
SDK version:rt-am335x-evm-04.03.00.05
kernel version:linux-rt 4.9.69
rs485…
Part Number: AM3352 Tool/software: For secure boot MPK and KEK are needed. I also find : "A one-time programmable memory location is usually set at the factory." and how to provide the keys to Ti.
As there is stated "usually" it implies other…
Hi Sreenivasa-san,
Thank you for your reply.
Daisuke Maeda said: Our customer is using a 3rd party RTOS and saw what appeared to be exceptions such as data abort and prefetch abort on the A8 core. They saw it on some of the same custom boards.
I suggested…
Part Number: AM3352 Tool/software: Hello TI support team.
I am trying to install CCS6.1.3(CCS6.1.3.00033_win32) on Windows 10. However, I get an error as shown in the image below.
7853.install_logs.zip
I am using Windows 10. However, I was able to install…
Part Number: AM3352 Tool/software: Hi
We use AM3352BZCZA100, and I need to use IO for input rising edge interrupt detection. Since the external input circuit involves EMC anti-interference design, if the filtering parameters are increased, there is a…
Hello Ito,
Here are some additional inputs i received:
This appears to me to be a driver issue. When they say “process interrupted” I can’t tell if they mean a physical CPU interrupt or some kind of single-threaded “I need to do something else for a bit…
Part Number: AM3352 Tool/software: We have a patch for BCH16 uboot nand driver, is a similar patch required for linux nand/mtd drivers; if we decide to write the nand paritions from within the linux.