Part Number: AM3354 Hello,
We are replacing the NAND flash on a custom AM3354-based board and are unable to boot the SPL/MLO directly from the new NAND device.
The old Toshiba NAND boots successfully on the same board design, but the new Foresee NAND…
Hello Marius
Below are some observations:
Signals that have specific direction can be indicated in the schematics for readability
capacitor voltage rating? Suggest enabling voltage rating
Is there a reason to have all the resistors reference designator…
Part Number: AM3354 Tool/software:
The "spl_nand_read" function in "spl_nand.c" use nand_page_size() to get NAND page size, but it's not initialized in SPL.
https://git.ti.com/cgit/ti-u-boot/ti-u-boot/tree/common/spl/spl_nand.c#n62
static ulong…
Part Number: AM3354 Hello TI Team,
We are experiencing an intermittent issue with SPI communication between AM3354 and an MRAM device. The problem occurs when using the McSPI controller with FIFO enabled.
Issue Description
Occasionally, the MISO…
Part Number: AM3354 Tool/software: I am using the 4.1 kernel on the AM3354 platform and have encountered an issue with USB tx FIFO clearing failure.
The logs that appear are as follows
以下作路径为高频次所需路径: 1.插入 USB 驱动器和 USB 打印机 2.通过 /dev/usb/lp0 向 USB…
Part Number: AM3354 Hi,
To fix the CVEs, I have upgraded SDK version to latest 09.03.05.02. The kernel version of this SDK is 6.1.119. I am suffering from a EMMC write timeout problem with fio test. This issue hasn't been observed in the old kernel…
Part Number: AM3354 Other Parts Discussed in Thread: PCA9535 Tool/software: 1. am 335x processor sdk 9.1 or 9.3 cross-compile tool
why choose to use external-toolchain-dir/arm-gnu-toolchain-11.3.rel1-x86_64-arm-none-linux-gnueabihf/bin/arm-none-linux…
Part Number: AM3354 Hi TI Team,
We have a customer who is evaluating the thermal performance of the AM3354BZCZ100 and would like to verify their Junction Temperature ( $T_j$ ) calculation.
Below are the measurement data and the calculation formula…
Part Number: AM3354 Team,
Our customer observes a watch dog reset at random times in AM3354x processsor
The status read from below register, which CPU reports that it is WD.
Base address for the PRM registers = 0x44E00000
Offset from the base…