Part Number: AM3356 Tool/software: Hi expert
We are facing a problem, please help
The SDK and kernel used are as follows: ・SDK Version.09.01.00.001 ・Linux Kernel Version.6.1.46(2023 LTS) We are considering disabling the SD card on the AM335x. To disable…
Part Number: AM3356 Hi expert
This is my first post.
When we configure the RTC settings, the following error may occur.
「rtc rtc1: __rtc_set_alarm: err=-22」
We not setting alarm.
Occurs when calling ioctl() with RTC_SET_TIME.
Why does it occur…
Part Number: AM3356 On SITARA the ethernet port interface name is "eth0" and "eth1" (in dual MAC mode).
I have a problem with the "eth1" name, because we already have some other network interface over USB for which we have already given the name "eth1…
Part Number: AM3356 Tool/software: Hi Team,
I have an inquiry from a customer who is running into intermittent failures on the AM3356:
"We are using the AM3356 processor from your company with IAR 8.4 compiler.
We are having some issue from the…
Part Number: AM3356 Tool/software: Hello team,
Just like we have a DDR3 tuning tool for AM335x, do we also have a similar tuning tool for DDR2 tuning on AM335x? If not, what is the best option my customer could take?
Regards,
Shashank
Part Number: AM3356 Other Parts Discussed in Thread: TPS65910 , AM3358
Tool/software:
We have replaces the AM335x processor on our board to one supporting 1Ghz . Previously we were running 800Mhz maximum and everything was fine..
With the new 1GHz…
Part Number: AM3356 Hi community,
i am just trying to run the profinet example on a Sitara processor AM3356. When i load the project i am able to build the example but if i try to debug these two error messages are displayed.
Do Someone has an idea…
Part Number: AM3356 Tool/software: Hello Team,
Hardware board : Custom board based on beaglebone reference.
SoC Used : AM3356 Uboot version : U-Boot SPL 2021.04 Linux kernel version : 5.4.188
SDRAM Used : W972GG6JB-25I SDRAM frequency : 266 MHz…
Part Number: AM3356 Tool/software: Hello everyone,I would like to seek your advice regarding a quality issue that has arisen after the installation of the AM3356BZCZD60 component. We have identified several types of quality issues, which we initially…
Part Number: AM3356 Tool/software: Hi expert,
My customers want to know when the Scarthgap for AM335x will be released. Could you tell me?
I saw the following url. e2e.ti.com/.../am3352-is-ti-scarthgap-build-feasible-as-of-2025-03-14
Our product…