Part Number: AM3357 According to the AM3357BZCZA80 datasheet (Page 103), the following power-down requirement is specified:
|VDDS - VDDSHVx| < 2 V
If |VDDS - VDDSHVx| temporarily exceeds 2 V during power-down, can the device tolerate this condition…
Part Number: AM3357 Other Parts Discussed in Thread: SYSCONFIG Dear TI Technical Support,
Could you please clarify the function assigned to pin U16 on the AM3357 ?
We found a discrepancy between the datasheet and the PinMux tool regarding the signal…
Part Number: AM3357 Continued from https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1633431/am3357-uart-driver-issue---am335x which was closed due to non-response on my part.
Kallikuppa Sreenivasa had written: Hello John,
…
Part Number: AM3357 Hello,
We want to use PTP with TI-RTOS (SYS/BIOS) on a custom board based on the AM3357, but are sample codes publicly available? If it exists, which version is it available from?
We are based on an older asset, version 4.02.00…
Part Number: AM3357 Hi Team,
Condition:
Customer is using am3357 connect fpga to transform data, base on this feature they are using gprmc to send the data.
Requirement:
Previous : sdk_01.01.02.01 with ccs 6.1.3
Current : sdk_6_03_00_106 …
Part Number: AM3357 Other Parts Discussed in Thread: SYSCONFIG We are considering a design using the AM3357 to implement 2-channel Ethernet and 1-channel EtherCAT on a single board.
Could you please confirm whether this configuration is feasible with…
Part Number: AM3357
Hi TI team,
I have a question regarding the Maximum Power Supply Slew Rate specification for the AM3357BZCZA80.
If the supply voltage has a non-linear rising waveform, as shown in the attached figure, should the slew rate be…
Part Number: AM3357 Hi Support Team,
Regarding the boot behavior, when SYSBOOT[15:14]=00b is set to select the 19.2MHz frequency and OSC0=24MHz is input, what behavior is assumed to occur? The phenomenon of not actually booting occurs on all boards…
Part Number: AM3357 Hi,
My customer has a question for power up sequence.
The datasheet shows the folloiwng power-up sequence in P.103.
The customer experiment the power-up sequence in their new system with AM3357BZCZD30 and TPS650xxRHBT PMIC…