Part Number: AM3505 Hi team,
Is it possible that the GPIO voltage varies with the AM3505 device temperature? For example, when the AM3505 temperature rises, does the GPIO voltage increase?
Sincerely. Ryu
Part Number: AM3505 Other Parts Discussed in Thread: FLASHTOOL Hi,
Customer download firmware to AM3505 on USB during boot.There is a USB driver in WIN-XP for connect to AM3505, but it can not used in WIN7. The USB driver is released in 2006, we doubt it…
Part Number: TPS65910 Other Parts Discussed in Thread: AM3505 Hi Team,
We are checking the PMIC alternate for AM3505/17 processor and we got the information from the TPS65910 datasheet ( https://www.ti.com/lit/ds/symlink/tps65910.pdf?ts=1657614107427&ref_url…
Part Number: AM3505 Other Parts Discussed in Thread: AM3517 Hi team,
My customer is considering using TPS650732RSLR as PMIC for AM3505. I’ve got an inquiry on the powering up sequence, could you take a look below?
On the Application note ( SLV…
Part Number: AM3505 We are using the ccdc interface on an am3505 processor.
The control register: Control_Devconf2 bit vpfe_pclk_invert_en has the following description:
0 Do not invert the pclk
1 Invert the pclk
My question is with a setting of 0 is…
Part Number: AM3505 Hi,
Quick question: Can you drop in a crypto enabled part (AM3505AZCNAC) in place of a non-crypto part (AM3505AZCNA) without any issues? Obviously assuming crypto accelerators are not used in the original design.
Thanks,
/ Wolfgang …
Part Number: AM3505 Hi Team,
The customer is using AM3505AZER with PHY and wants to know the internal pull-up/down register value which is including the variation
Would you please provide it?
There is II : Input current for dual voltage IO pins specification…
Part Number: AM3505 Hello.
Section 24.4.7.6 of the TRM states that it supports MMC Specification v4.2.
Can you confirm if we can use later versions of this MMC specification with the AM3505?
Thanks.
Part Number: AM3505 Hi All
Are there any known cases of the eMMC chip to go into INACTIVE state
We are using AM3505 and eMMC from different vendors, in some units it looks like the eMMC has changed state into INACTIVE mode after have being initialized…