Part Number: AM3505 Other Parts Discussed in Thread: TPS65910 ,
A bit of background info : the 26 MHz sys_clk is generated by an external oscillator, which is enabled when sys_clkreq asserts from the Sitara.
Observing on Oscope, sys_clkreq asserts ( a…
Part Number: AM3505
Tool/software: Linux
The issue happened in the kernel 2.6. We have a app that communicate with DSP through UART port. If we used reboot command to reboot reader, sometimes app failed communicate with DSP. We measured the signal on line…
Part Number: AM3505 Customer using AM3505BZCNA and currently debugging a GPMC issue. They have identified that they did not tie pin G20 and G21 to GND, and they will fix that in the next board spin. What they want to know is the GPMC issue they are having…
Part Number: AM3505 Customer in production but is mandated to switch to Win10. Using Flash Tools v1.6 to program AM3505 system over USB (previously WinXP) but tool is not working on 64 bit Win10. Tried both running in XP Compatibility mode as well as…
Part Number: AM3505 Tool/software: Linux Q1: We have been experiencing a random kernel crash on our radio with AM3505 and Kernel 2.6.37 and wondering if any patches from TI could be involved?
Even if this isn't relevant to Texas Instruments would appreciate…
Part Number: AM3505 Tool/software: Linux Hi,
I am using AM3505 Processor and I am using 4.9 kernel.
Did Armv7 affected with bounds check bypass, Spectre-V1, Spectre 1.0 and branch target injection, Spectre-V2.
if yes then is there any fix is available…
Part Number: AM3505 Other Parts Discussed in Thread: AM3358 ,
Hi,
I represent the Organization Tekever Space and we are using your products.
For the your project, that we're developing we use the AM3505 and AM3358
I needed to know if some of this products…
Part Number: AM3505 Team, regarding the AM3505 -- can you confirm that AM3505AZCNA & AM3505AZCNA C are 100% pin-pin drop in compatible with no hardware changes needed to move between the parts? I have been looking in chapter 7 of the datasheet as well…
Part Number: AM3505
Team, we are working with a customer trying to connect to the AM3505 via JTAG. They are asking about SCAN_N and I believe our equivalent instruction is EXTEST but I am not on sure footing here. Are there any documents I should be…
Part Number: AM3505
Hi,
I want to set GPIO_96 as an output and drive that pin high using JTAG
How can i do this or which section in the datasheet has the relevant information? Thanks