Part Number: AM3505
Dear E2E Support,
My customer has some start-up issue with our TPS65023 which power our AM3505 .
Here is his description below:
On scope 5 :
- Yellow trace => +5V_ALIM (Main Power supply of the PMIC)
- red Trace => +1.8V (Power…
Part Number: AM3505 Other Parts Discussed in Thread: AM3517
Tool/software: Linux
Our board use AM3505 + Linux 2.6 kernel. After board power on.
I unplug and plug rtl8187 USB WiFi dongle multi times, and got following messages:
hub 1-0:1.0: port 1 disabled…
Part Number: AM3505
Tool/software: Code Composer Studio
Hi
I am just starting from scratch, i need to configure an I/O to output high, i know the steps to configure the I/O (registers), but the problem is need to do this using JTAG
I couldn't find enough…
Part Number: TPS65023 Other Parts Discussed in Thread: AM3505 , TPS650250 Dear E2E Support,
My cutomer has some start-up issue with our TPS65023 which power our AM3505.
Here is his description below:
On scope 5 :
- Yellow trace => +5V_ALIM (Main Power…
Part Number: AM3505
Hi All,
in our design we are using 32Khz external as SYS_32K clock and 26MHz for SYS_XTALIN
is there any register available in the processor which would store/detect these clock frequencies for production testing? we are trying to…
Part Number: AM3505
Dear Sir/Madam,
I read through the AM3505 TRM and found the statement circled in RED below. want to clarify:
1. Does GP device means AM3505AZCNA? so AM3505AZCNAC is not consider GP device? or it means production device as compare to…
Part Number: AM3505 Tool/software: Starterware Hello,
Starterware for am33x contains eDMA.
Is it possible to modify these code to be used as sDMA for other processor (am35) or will it require too much effort ?
Thank you,
Ran
Part Number: AM3505
Hi,
I have a AM3505 processor using the GPMC interface to interface a FPGA. I am trying to setup the timing constraints inside the FPGA to match the GPMC configuration. I have a doubt while reading the AM3505 datasheet (http://www…