Other Parts Discussed in Thread: AM3871 Hello,
Does AM3871 support PMU(Performance Monitoring Unit) ?
OMAP4 seems to have PMU.
http://e2e.ti.com/support/omap/f/849/t/184885.aspx
But I can't find any PMU related document on AM3871 datasheet.
I want…
Other Parts Discussed in Thread: AM3874 , AM3871AM3871 Sitara ARM still shows in preview status. Do you know when TI is targeting production release? The AM3874 is now released as the pre-production XAM3874 version, but the other AM387x are not.
Hello,
The device data sheet describes this as "source asynchronous transmit clock" in (G)MII mode (pp 46, 51). In the Technical Reference Manual, it is defined as being synchronous (pp 1093, 1094). Can you clear this up?
Also, figure 8-9…
The spreadsheet on the wiki for the DM814x and AM387x, http://processors.wiki.ti.com/index.php/DM814x_AM387x_Power_Estimation , only has DM814x parts in the drop-down menu. Where is the power estimation for the AM387x Sitara parts?
Other Parts Discussed in Thread: AM3871
Hello,
I couldn't find IBIS Model for AM3871 in the product product.
Could you please let us know when does TI releases the IBIS Model.
If possible could you please send us the preliminary version.
(our…
Other Parts Discussed in Thread: AM3871 , AM3874
Hi,
We don’t need the Media controller /HDVPSS/ISS in AM3872, however we want those pins to be usable as GPIO.
Is AM3871 a better alternate for us?
Regards, Abhishek
Other Parts Discussed in Thread: AM3871am3871 hard design:
in the am3871 data sheet 7.2.8: " The 3.3 V supplies must never be more than 2 V above the 1.8 V ."
Can I power-up 1.8V first,then power-up 3.3V? I can add a diode between 1.8V and 3.3V. The anode…
Hi Field team.
Please refer below inputs:
1. Can I share the schematics for review over E2E
We do not support schematics review request by field teams or customer over E2E. TI field team will have to submit schematics review request over email after reviewing…
Other Parts Discussed in Thread: AM3871 My system is linux-2.6.37-psp04.04.00.01-sk running on am3871, I'm using USB-Ethernet / RNDIS gadget to communicate with Windows 7/8.1 PC. It works fine with desktop or notebook PC, but not with tablet. When connecting…