Part Number: AM3892 Tool/software: Linux Hi,
The AM3892 Datasheet specifies that the resistance of the HDMI_EXTSWING line should be 6.8 kohm.
But, the EVM Board is connected at 5.9 kohm.
Please let me know which is correct.
BR,
Part Number: AM3892 Customer using EZSDK 5_04_00_11
The problem they have is that CPU does not receive an interrupt of reception of Ethernet packet on EMAC0 port.
During it, CPU can send a packet through EMAC0. The problem is only on receive direction…
Hi,
Just an confirmation about the errata Advisory 2.0.68. Advisory 2.0.68: Continuous Writes From Cortex-A8 Occasionally Starve Other Requestors for DDR Bandwidth .
We would like to confirm if the above Errata is FIXED in the latest Silicon Revision…
Other Parts Discussed in Thread: AM3892 , CCSTUDIO I'm writing a BSP for an SD Card driver, and encountered an issue which is preventing me from reading data from the SD Card.
The SD Card driver is attempting to read the SCR from the card using CMD51…
Other Parts Discussed in Thread: AM3892 Hello,
We are using ARM AM3892 Sitara processor in our customized design,
We have two Boot mode option,1) NAND Boot, 2) SD Boot,
We have configured to SD Boot mode in our design,
We are getting SD clock…
Other Parts Discussed in Thread: AM3892 Hi Paul,
I am sorry to post this question here.
We would like to know if this kind of clock delay feature necessary for GMII interface(on AM3892). I have posted the the question on Davinci forum but not getting…
Other Parts Discussed in Thread: AM3892 Hi Miroslav,
really appreciate your response.
I am also working with same chip and AM3892 on Uboot and Linux kernel side.
Uboot: GPMC is connected with Nand flash chip(MT29F16G08ABACAWP). I have already modified…