Part Number: AM4372 Hi Team,
My customer is running for POS machine.
Please help to suggest TI processor P/N for POS will can be used to pass Payment Card Industry Data Security Standard 4.0(PCI 4.0).
Thanks.
Part Number: AM4372 Hi experts,
My customer wants to implement Deepsleep using "PROCESSOR-SDK-LINUX-AM437X v: 06.03.00.106".
Q1:Is it possible to WakeUp with GPIO0 from Deepsleep on AM437x? I'm confused because the descriptions are different…
Hi,
Apologies for the delay.
Kotaro Yamashita said: 1) Waiting for existing number of data. For now, customer accpepted to use your suggestion. For hold time, they can use below?
RDACCESSTIME + 1 GPMC_FCLK = CSRDOFFTIME (= OEOFFTIME)
Yes. I you can use…
Part Number: AM4372 Hi,
For USB device mode of AM4372, what is USB_VBUS valid threshold voltage?
In datasheet, it seems to be 4.4V.
However, USB host can supply 3.3V now and in this case, AM4372 works well as USB device mode.
Is there any problem?
Thanks…
Part Number: AM4372 Other Parts Discussed in Thread: SYSBIOS Hi everyone,
I am currently using Uart0 and Uart2 to communicate with 2 different devices.
This is the configuration of the Uarts:
off_board_uart0_pins_default: uart0_pins_default { pinctrl…
Part Number: AM4372
Hi,
We are using yocto 07_03_00_005 PSDK version and it supports 5.10.100 kernel. We want to know, What is the latest LKML version supported for AM4372. Please let us know.
Thanks,
M.Mahesh.
Part Number: AM4372 I'd like to design a system based on the AM4372 SOC.
I'd like the GPMC bus to be clocked with an external oscillator that has a frequency of 43.75 MHz.
Does this device support that ?
Part Number: AM4372 Hi,
I am using TI SDK "proc-sdk-secdev-am437x-hs-evm-01.06.00.05" to build the MLO file but It doesnt work(i.e. no serial output).
Could you provide more explanation how to verify the address "ISW_LOAD_ADDR" passed to the…